TIOVX User Guide
vx_event_node_error Struct Reference

Parameter structure returned with event of type VX_EVENT_NODE_ERROR. More...

#include <vx_khr_pipelining.h>

Data Fields

vx_graph graph
 graph which generated this event
 
vx_node node
 node which generated this event
 
vx_status status
 error condition of node
 

Detailed Description

Parameter structure returned with event of type VX_EVENT_NODE_ERROR.

Definition at line 404 of file vx_khr_pipelining.h.


The documentation for this struct was generated from the following file: