TIOVX User Guide
vx_event_graph_parameter_consumed Struct Reference

Parameter structure returned with event of type VX_EVENT_GRAPH_PARAMETER_CONSUMED. More...

#include <vx_khr_pipelining.h>

Data Fields

vx_graph graph
 graph which generated this event
 
vx_uint32 graph_parameter_index
 graph parameter index which generated this event
 

Detailed Description

Parameter structure returned with event of type VX_EVENT_GRAPH_PARAMETER_CONSUMED.

Definition at line 368 of file vx_khr_pipelining.h.


The documentation for this struct was generated from the following file: