TIOVX User Guide

H3A AEW configuration data structure used by the TIVX_KERNEL_VISS kernel. More...

#include <hwa_vpac_viss.h>

Data Fields

uint16_t aewwin1_WINH
 
uint16_t aewwin1_WINW
 
uint16_t aewwin1_WINVC
 
uint16_t aewwin1_WINHC
 
uint16_t aewsubwin_AEWINCV
 
uint16_t aewsubwin_AEWINCH
 

Detailed Description

H3A AEW configuration data structure used by the TIVX_KERNEL_VISS kernel.

This is included in the tivx_h3a_data_t H3A output if the AEWB mode of H3A was enabled. This is included in case the 2A algorithm needs to know the configuration that the VISS used for the H3A AEWB engine.

Definition at line 224 of file hwa_vpac_viss.h.

Field Documentation

◆ aewwin1_WINH

uint16_t tivx_h3a_aew_config::aewwin1_WINH

AEW Window Height

Definition at line 227 of file hwa_vpac_viss.h.

◆ aewwin1_WINW

uint16_t tivx_h3a_aew_config::aewwin1_WINW

AEW Window Width

Definition at line 229 of file hwa_vpac_viss.h.

◆ aewwin1_WINVC

uint16_t tivx_h3a_aew_config::aewwin1_WINVC

AEW Vertical Count

Definition at line 231 of file hwa_vpac_viss.h.

◆ aewwin1_WINHC

uint16_t tivx_h3a_aew_config::aewwin1_WINHC

AEW Horizontal Count

Definition at line 233 of file hwa_vpac_viss.h.

◆ aewsubwin_AEWINCV

uint16_t tivx_h3a_aew_config::aewsubwin_AEWINCV

AEW Subwindow Vertical Increment Value

Definition at line 235 of file hwa_vpac_viss.h.

◆ aewsubwin_AEWINCH

uint16_t tivx_h3a_aew_config::aewsubwin_AEWINCH

AEW Subwindow Horizontal Increment Value

Definition at line 237 of file hwa_vpac_viss.h.


The documentation for this struct was generated from the following file: