TIOVX User Guide

BAM plugin definition. More...

#include <tivx_bam_kernel_wrapper.h>

Data Fields

const BAM_KernelInfo * kernelInfo
 
const BAM_KernelHelperFuncDef * kernelHelperFunc
 
const BAM_KernelExecFuncDef * kernelExecFunc
 
const char * name
 

Detailed Description

BAM plugin definition.

Used for registering a BAM plugin with OpenVX on the DSPs.

Definition at line 160 of file tivx_bam_kernel_wrapper.h.

Field Documentation

◆ kernelInfo

const BAM_KernelInfo* tivx_bam_plugin_def::kernelInfo

Pointer to the kernel's contextual information structure BAM_KernelInfo

Definition at line 162 of file tivx_bam_kernel_wrapper.h.

◆ kernelHelperFunc

const BAM_KernelHelperFuncDef* tivx_bam_plugin_def::kernelHelperFunc

Pointer to the structure BAM_KernelHelperFuncDef that list the helper functions

Definition at line 163 of file tivx_bam_kernel_wrapper.h.

◆ kernelExecFunc

const BAM_KernelExecFuncDef* tivx_bam_plugin_def::kernelExecFunc

Pointer to the structure BAM_KernelExecFuncDef that list the execution functions

Definition at line 164 of file tivx_bam_kernel_wrapper.h.

◆ name

const char* tivx_bam_plugin_def::name

Unique name of the kernel plugin

Definition at line 165 of file tivx_bam_kernel_wrapper.h.


The documentation for this struct was generated from the following file: