![]() |
TIOVX User Guide
|
Data corresponding to results of 2A algorithm. More...
#include <hwa_vpac_viss.h>
Data Fields | |
| uint32_t | h3a_source_data |
| uint32_t | exposure_time |
| uint32_t | analog_gain |
| uint32_t | ae_valid |
| uint32_t | ae_converged |
| uint32_t | digital_gain |
| uint32_t | wb_gains [4] |
| int32_t | wb_offsets [4] |
| uint32_t | color_temperature |
| uint32_t | awb_valid |
| uint32_t | awb_converged |
Data corresponding to results of 2A algorithm.
Macro to enable all VISS error events (including platform-specific)
This is the data structure used for the ae_awb_result parameter of tivxVpacVissNode. This is used by the VISS to index into the appropriate photospace in the DCC database.
Definition at line 449 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::h3a_source_data |
Indicates the source data corresponding to this data:
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_H3A_IN_RAW0 | H3A Input is from RAW0 |
| TIVX_VPAC_VISS_H3A_IN_RAW1 | H3A Input is from RAW1 |
| TIVX_VPAC_VISS_H3A_IN_RAW2 | H3A Input is from RAW2 |
| TIVX_VPAC_VISS_H3A_IN_LSC | H3A Input is from LSC |
| TIVX_VPAC_VISS_H3A_IN_PCID | H3A Input is from PCID |
TIVX_VPAC_VISS_H3A_IN_PCID is applicable for only VPAC3L
Definition at line 460 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::exposure_time |
Measured in micro seconds (us)
Definition at line 462 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::analog_gain |
Analog Gain
Definition at line 464 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::ae_valid |
Is AE output valid?
Definition at line 466 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::ae_converged |
Is AE converged?
Definition at line 468 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::digital_gain |
Digital Gain
Definition at line 470 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::wb_gains[4] |
White Balance Gains
Definition at line 472 of file hwa_vpac_viss.h.
| int32_t tivx_ae_awb_params_t::wb_offsets[4] |
White Balance Offsets
Definition at line 474 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::color_temperature |
Color Temperature (K)
Definition at line 476 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::awb_valid |
Is AWB output valid?
Definition at line 478 of file hwa_vpac_viss.h.
| uint32_t tivx_ae_awb_params_t::awb_converged |
Is AWB converged?
Definition at line 480 of file hwa_vpac_viss.h.