TIOVX User Guide
tiovx.enums.Direction Class Reference

Parameter direction (OpenVX equivalent = vx_direction_e) More...

Inherits Enum.

Static Public Attributes

int INPUT = 1
 OpenVX equivalent = VX_INPUT.
 
int OUTPUT = 2
 OpenVX equivalent = VX_OUTPUT.
 
int BIDIRECTIONAL = 3
 OpenVX equivalent = VX_BIDIRECTIONAL.
 

Detailed Description

Parameter direction (OpenVX equivalent = vx_direction_e)

Example usage:
Direction.INPUT
Direction.OUTPUT

Definition at line 739 of file enums.py.


The documentation for this class was generated from the following file: