89 #define SDL_VIM_MAX_INTR_GROUPS (32U) 92 #define SDL_VIM_NUM_INTRS_PER_GROUP (32U) 111 #define SDL_VIM_INTR_TYPE_LEVEL ((uint32_t)0U) 114 #define SDL_VIM_INTR_TYPE_PULSE ((uint32_t)1U) 133 #define SDL_VIM_INTR_MAP_IRQ ((uint32_t)0U) 136 #define SDL_VIM_INTR_MAP_FIQ ((uint32_t)1U) 139 #define SDL_VIM_INTR_MAP_ALL ((uint32_t)2U) uint32_t SDL_VIM_getRevision(SDL_vimRegs *pRegs)
Return revision of the VIM module.
int32_t SDL_VIM_clrIntrPending(SDL_vimRegs *pRegs, uint32_t intrNum)
Clear the raw interrupt status bit for the specified interrupt.
uint32_t SDL_VimIntrMap
This enumerator defines the possible output interrupt types. Each source interrupt can be configured ...
Definition: sdl_vim.h:124
void SDL_VIM_setDedVectorAddr(SDL_vimRegs *pRegs, uint32_t dedVectorAddr)
Set the DED interrupt vector address.
int32_t SDL_VIM_getDedVectorAddr(SDL_vimRegs *pRegs, uint32_t *pDedVectorAddr)
Get the DED interrupt vector address.
#define SDL_VIM_MAX_INTR_GROUPS
Definition: sdl_vim.h:89
int32_t SDL_VIM_ackIntr(SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap)
Acknowledge servicing is complete for the specified interrupt type.
int32_t SDL_VIM_getIntrType(SDL_vimRegs *pRegs, uint32_t intrNum)
Get the interrupt type.
int32_t SDL_VIM_getActivePendingIntr(SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap, uint32_t *pIntrNum, uint32_t *pPri)
Get information on the current highest priority pending interrupt.
uint32_t SDL_VIM_getIrqVectorAddress(SDL_vimRegs *pRegs)
Get the current IRQ vector address.
uint32_t SDL_VIM_getNumIntrs(SDL_vimRegs *pRegs)
Get the number of interrupts supported by this VIM.
volatile uint32_t INTTYPE
Definition: sdl_vim.h:159
uint32_t SDL_VIM_getGroupsIntrPending(SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap)
Get bit-mask of masked interrupt status for all interrupt groups.
volatile uint32_t INTR_EN_CLR
Definition: sdl_vim.h:157
volatile uint32_t PID
Definition: sdl_vim.h:171
volatile uint32_t INTR_EN_SET
Definition: sdl_vim.h:156
uint32_t SDL_VIM_getFiqVectorAddress(SDL_vimRegs *pRegs)
Get the current FIQ vector address.
#define SDL_VIM_NUM_INTRS_PER_GROUP
Definition: sdl_vim.h:92
int32_t SDL_VIM_setIntrPending(SDL_vimRegs *pRegs, uint32_t intrNum)
Set the raw interrupt status bit for the specified interrupt.
uint32_t SDL_VimIntrType
This enumerator defines the possible interrupt types. Each source interrupt is either an active high ...
Definition: sdl_vim.h:102
int32_t SDL_VIM_verifyCfgIntr(SDL_vimRegs *pRegs, uint32_t intrNum, uint32_t pri, SDL_VimIntrMap intrMap, SDL_VimIntrType intrType, uint32_t vecAddr)
Read back Verify Configure a source interrupt.
int32_t SDL_VIM_getStaticRegs(SDL_vimRegs *pRegs, SDL_vimStaticRegs *pStaticRegs)
Read back of static registers for VIM.
uint32_t SDL_VIM_getGroupIntrPending(SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap, uint32_t groupNum, bool bMasked)
Get bit-mask of raw or masked interrupt status for all interrupts within a group.
This structure defines the static register groups identified for VIM.
Definition: sdl_vim.h:167
This structure defines the group registers identified for VIM static registers.
Definition: sdl_vim.h:155
volatile uint32_t INTMAP
Definition: sdl_vim.h:158
int32_t SDL_VIM_cfgIntr(SDL_vimRegs *pRegs, uint32_t intrNum, uint32_t pri, SDL_VimIntrMap intrMap, SDL_VimIntrType intrType, uint32_t vecAddr)
Configure a source interrupt using VIM.
int32_t SDL_VIM_setIntrEnable(SDL_vimRegs *pRegs, uint32_t intrNum, bool bEnable)
Enable or disable interrupt status mask for the specified interrupt.
volatile uint32_t INFO
Definition: sdl_vim.h:172