SDL API Guide for J721E
VIM Functions

Introduction

Functions

uint32_t SDL_VIM_getRevision (SDL_vimRegs *pRegs)
 Return revision of the VIM module. More...
 
uint32_t SDL_VIM_getNumIntrs (SDL_vimRegs *pRegs)
 Get the number of interrupts supported by this VIM. More...
 
int32_t SDL_VIM_cfgIntr (SDL_vimRegs *pRegs, uint32_t intrNum, uint32_t pri, SDL_VimIntrMap intrMap, SDL_VimIntrType intrType, uint32_t vecAddr)
 Configure a source interrupt using VIM. More...
 
int32_t SDL_VIM_verifyCfgIntr (SDL_vimRegs *pRegs, uint32_t intrNum, uint32_t pri, SDL_VimIntrMap intrMap, SDL_VimIntrType intrType, uint32_t vecAddr)
 Read back Verify Configure a source interrupt. More...
 
int32_t SDL_VIM_getIntrType (SDL_vimRegs *pRegs, uint32_t intrNum)
 Get the interrupt type. More...
 
void SDL_VIM_setDedVectorAddr (SDL_vimRegs *pRegs, uint32_t dedVectorAddr)
 Set the DED interrupt vector address. More...
 
int32_t SDL_VIM_getDedVectorAddr (SDL_vimRegs *pRegs, uint32_t *pDedVectorAddr)
 Get the DED interrupt vector address. More...
 
int32_t SDL_VIM_getActivePendingIntr (SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap, uint32_t *pIntrNum, uint32_t *pPri)
 Get information on the current highest priority pending interrupt. More...
 
uint32_t SDL_VIM_getIrqVectorAddress (SDL_vimRegs *pRegs)
 Get the current IRQ vector address. More...
 
uint32_t SDL_VIM_getFiqVectorAddress (SDL_vimRegs *pRegs)
 Get the current FIQ vector address. More...
 
uint32_t SDL_VIM_getGroupsIntrPending (SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap)
 Get bit-mask of masked interrupt status for all interrupt groups. More...
 
uint32_t SDL_VIM_getGroupIntrPending (SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap, uint32_t groupNum, bool bMasked)
 Get bit-mask of raw or masked interrupt status for all interrupts within a group. More...
 
int32_t SDL_VIM_setIntrPending (SDL_vimRegs *pRegs, uint32_t intrNum)
 Set the raw interrupt status bit for the specified interrupt. More...
 
int32_t SDL_VIM_clrIntrPending (SDL_vimRegs *pRegs, uint32_t intrNum)
 Clear the raw interrupt status bit for the specified interrupt. More...
 
int32_t SDL_VIM_ackIntr (SDL_vimRegs *pRegs, SDL_VimIntrMap intrMap)
 Acknowledge servicing is complete for the specified interrupt type. More...
 
int32_t SDL_VIM_setIntrEnable (SDL_vimRegs *pRegs, uint32_t intrNum, bool bEnable)
 Enable or disable interrupt status mask for the specified interrupt. More...
 
int32_t SDL_VIM_getStaticRegs (SDL_vimRegs *pRegs, SDL_vimStaticRegs *pStaticRegs)
 Read back of static registers for VIM. More...
 

Function Documentation

◆ SDL_VIM_getRevision()

uint32_t SDL_VIM_getRevision ( SDL_vimRegs *  pRegs)

Return revision of the VIM module.

This function returns the contents of the VIM revision register. Consult the VIM module documentation for a description of the contents of the revision register.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
Returns
The 32-bit revision register is returned.

◆ SDL_VIM_getNumIntrs()

uint32_t SDL_VIM_getNumIntrs ( SDL_vimRegs *  pRegs)

Get the number of interrupts supported by this VIM.

This function returns the number of interrupts supported by this VIM. This value is always a multiple of 32.

The number of interrupt groups = number of interrupts / 32.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
Returns
The number of interrupts supported

◆ SDL_VIM_cfgIntr()

int32_t SDL_VIM_cfgIntr ( SDL_vimRegs *  pRegs,
uint32_t  intrNum,
uint32_t  pri,
SDL_VimIntrMap  intrMap,
SDL_VimIntrType  intrType,
uint32_t  vecAddr 
)

Configure a source interrupt using VIM.

This function configures the specified source interrupt per the provided parameters.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrNum[IN] Interrupt number (0..SDL_VIM_getNumIntrs()-1)
pri[IN] Interrupt priority (0(highest)..15(lowest))
intrMap[IN] Interrupt mapping (SDL_VIM_INTR_MAP_IRQ or SDL_VIM_INTR_MAP_FIQ, see SDL_VimIntrMap)
intrType[IN] Interrupt type (SDL_VIM_INTR_TYPE_LEVEL or SDL_VIM_INTR_TYPE_PULSE, see SDL_VimIntrType)
vecAddr[IN] 32-bit vector address (forced to 32-bit alignment)
Returns
0 = success -1 = intrNum or pri parameters are out of range

◆ SDL_VIM_verifyCfgIntr()

int32_t SDL_VIM_verifyCfgIntr ( SDL_vimRegs *  pRegs,
uint32_t  intrNum,
uint32_t  pri,
SDL_VimIntrMap  intrMap,
SDL_VimIntrType  intrType,
uint32_t  vecAddr 
)

Read back Verify Configure a source interrupt.

This function verifies the writetn configuration of interrupt for the specified source interrupt per the provided parameters.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrNum[IN] Interrupt number (0..SDL_VIM_getNumIntrs()-1)
pri[IN] Interrupt priority (0(highest)..15(lowest))
intrMap[IN] Interrupt mapping (SDL_VIM_INTR_MAP_IRQ or SDL_VIM_INTR_MAP_FIQ, see SDL_VimIntrMap)
intrType[IN] Interrupt type (SDL_VIM_INTR_TYPE_LEVEL or SDL_VIM_INTR_TYPE_PULSE, see SDL_VimIntrType)
vecAddr[IN] 32-bit vector address (forced to 32-bit alignment)
Returns
0 = success (matches to expected values) -1 = VIM register configuration is not matching expected value

◆ SDL_VIM_getIntrType()

int32_t SDL_VIM_getIntrType ( SDL_vimRegs *  pRegs,
uint32_t  intrNum 
)

Get the interrupt type.

This function returns the interrupt type for the specified interrupt number.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrNum[IN] Interrupt number (0..SDL_VIM_getNumIntrs()-1)
Returns
0 = SDL_VIM_INTR_TYPE_LEVEL 1 = SDL_VIM_INTR_TYPE_PULSE -1 = intrNum parameter is out of range

◆ SDL_VIM_setDedVectorAddr()

void SDL_VIM_setDedVectorAddr ( SDL_vimRegs *  pRegs,
uint32_t  dedVectorAddr 
)

Set the DED interrupt vector address.

This function sets the 32-bit interrupt vector address (the address must be 32-bit aligned) of an interrupt to be used if an uncorrectable double-bit error (DED) is detected in any of the interrupt vector addresses. If there is a DED, the pVectorAddr argument of the SDL_VIM_getActivePendingIntr function will be populated with the value in this field instead of their normal vector.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
dedVectorAddr[IN] The 32-bit DED interrupt vector address

◆ SDL_VIM_getDedVectorAddr()

int32_t SDL_VIM_getDedVectorAddr ( SDL_vimRegs *  pRegs,
uint32_t *  pDedVectorAddr 
)

Get the DED interrupt vector address.

This function sets the 32-bit interrupt vector address (the address must be 32-bit aligned) of an interrupt to be used if an uncorrectable double-bit error (DED) is detected in any of the interrupt vector addresses. If there is a DED, the pVectorAddr argument of the SDL_VIM_getActivePendingIntr function will be populated with the value in this field instead of their normal vector.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
pDedVectorAddr[OUT] Pointer to the 32-bit DED interrupt vector address
Returns
0 = Success SDL_ESYS_FAIL = Failure

◆ SDL_VIM_getActivePendingIntr()

int32_t SDL_VIM_getActivePendingIntr ( SDL_vimRegs *  pRegs,
SDL_VimIntrMap  intrMap,
uint32_t *  pIntrNum,
uint32_t *  pPri 
)

Get information on the current highest priority pending interrupt.

This function returns information on the current highest priority pending interrupt. The SDL_VIM_getIrqVectorAddress or SDL_VIM_getFiqVectorAddress functions can be called to get the vector address associated with the pending interrupt.

There are two types of pending interrupts that can be queried: SDL_VIM_INTR_MAP_IRQ or SDL_VIM_INTR_MAP_FIQ (see SDL_VimIntrMap).

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrMap[IN] Type of active interrupt to query (see SDL_VimIntrMap)
pIntrNum[OUT] Pointer where interrupt number is returned
pPri[OUT] Pointer where priority of interrupt is returned
Returns
0 = success -1 = no interrupt is currently pending

◆ SDL_VIM_getIrqVectorAddress()

uint32_t SDL_VIM_getIrqVectorAddress ( SDL_vimRegs *  pRegs)

Get the current IRQ vector address.

This function returns the 32-bit interrupt vector address of the currently pending IRQ interrupt.

Note that the vector address returned is valid only if there is a pending interrupt.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
Returns
Interrupt vector address of the currently pending IRQ interrupt

◆ SDL_VIM_getFiqVectorAddress()

uint32_t SDL_VIM_getFiqVectorAddress ( SDL_vimRegs *  pRegs)

Get the current FIQ vector address.

This function returns the 32-bit interrupt vector address of the currently pending FIQ interrupt.

Note that the vector address returned is valid only if there is a pending interrupt.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
Returns
Interrupt vector address of the currently pending FIQ interrupt or 0 if there is no FIQ interrupt pending

◆ SDL_VIM_getGroupsIntrPending()

uint32_t SDL_VIM_getGroupsIntrPending ( SDL_vimRegs *  pRegs,
SDL_VimIntrMap  intrMap 
)

Get bit-mask of masked interrupt status for all interrupt groups.

This function returns a 32-bit mask of the masked interrupt status for all interrupt groups, where bit # M in the mask indicates the masked interrupt status for interrupt group M (0 = no interrupt pending for that group, 1 = interrupt is pending for that group).

Group M aggregates the interrupt status for interrupt numbers 32*M ... (32*M)+31. The SDL_VIM_getGroupIntrPending function can be called to return a bit-mask of the raw or masked interrupt status for all 32 interrupts in a group.

There are two types of pending interrupts that can be queried: SDL_VIM_INTR_MAP_IRQ or SDL_VIM_INTR_MAP_FIQ (see SDL_VimIntrMap).

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrMap[IN] Type of interrupt to query (see SDL_VimIntrMap)
Returns
A 32-bit mask indicates which groups of interrupts have pending, unmasked interrupts

◆ SDL_VIM_getGroupIntrPending()

uint32_t SDL_VIM_getGroupIntrPending ( SDL_vimRegs *  pRegs,
SDL_VimIntrMap  intrMap,
uint32_t  groupNum,
bool  bMasked 
)

Get bit-mask of raw or masked interrupt status for all interrupts within a group.

This function returns a 32-bit mask of the raw or masked interrupt status for all interrupts within the specified interrupt group, where bit # N in the mask indicates the pending interrupt status for interrupt source (32*groupNum)+N (0 = no interrupt pending, 1 = interrupt is pending).

The SDL_VIM_getGroupsIntrPending function can be called to return a bit-mask of the masked interrupt status for all 32 interrupt groups.

If bMasked is false, the raw interrupt status is returned. If bMasked is true, then intrMap determines the type of masked interrupt status returned as follows: SDL_VIM_INTR_MAP_IRQ = Masked IRQ interrupt status SDL_VIM_INTR_MAP_FIQ = Masked FIQ interrupt status SDL_VIM_INTR_MAP_ALL = Masked IRQ and FIQ interrupt status

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrMap[IN] Type of interrupt to query (see SDL_VimIntrMap)
groupNum[IN] Interrupt group number (0..31)
bMasked[IN] false = return raw interrupt status true = return masked interrupt status
Returns
A 32-bit mask of the raw or masked interrupt status for all interrupts within the group specified by groupNum

◆ SDL_VIM_setIntrPending()

int32_t SDL_VIM_setIntrPending ( SDL_vimRegs *  pRegs,
uint32_t  intrNum 
)

Set the raw interrupt status bit for the specified interrupt.

This function forcibly sets the raw interrupt status bit for the specified interrupt number.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrNum[IN] Interrupt number (0..SDL_VIM_getNumIntrs()-1)
Returns
0 = success -1 = intrNum is out of range

◆ SDL_VIM_clrIntrPending()

int32_t SDL_VIM_clrIntrPending ( SDL_vimRegs *  pRegs,
uint32_t  intrNum 
)

Clear the raw interrupt status bit for the specified interrupt.

This function clears the raw interrupt status bit for the specified interrupt number.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrNum[IN] Interrupt number (0..SDL_VIM_getNumIntrs()-1)
Returns
0 = success -1 = intrNum is out of range

◆ SDL_VIM_ackIntr()

int32_t SDL_VIM_ackIntr ( SDL_vimRegs *  pRegs,
SDL_VimIntrMap  intrMap 
)

Acknowledge servicing is complete for the specified interrupt type.

The function is used to acknowlege that the specified interrupt type has been serviced. The VIM will then re-evaluate the new highest priority interrupt.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrMap[IN] Interrupt map type (see SDL_VimIntrMap)
Returns
0 = success -1 = intrMap is out of range

◆ SDL_VIM_setIntrEnable()

int32_t SDL_VIM_setIntrEnable ( SDL_vimRegs *  pRegs,
uint32_t  intrNum,
bool  bEnable 
)

Enable or disable interrupt status mask for the specified interrupt.

The function is used to enable or disable the interrupt status mask for the specified interrupt. Interrupt sources with an enabled mask are used in the generation of the output IRQ or FIQ interrupt. Interrupt sources with a disabled mask are not used in the generation of the output IRQ or FIQ interrupt.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
intrNum[IN] Interrupt number (0..SDL_VIM_getNumIntrs()-1)
bEnable[IN] false = disable interrupt status mask true = enable interrupt status mask
Returns
0 = success -1 = intrNum is out of range

◆ SDL_VIM_getStaticRegs()

int32_t SDL_VIM_getStaticRegs ( SDL_vimRegs *  pRegs,
SDL_vimStaticRegs pStaticRegs 
)

Read back of static registers for VIM.

The function is used to acknowlege that the specified interrupt type has been serviced. The VIM will then re-evaluate the new highest priority interrupt.

Parameters
pRegs[IN] Pointer to the SDL_vimRegs register structure
pStaticRegs[IN] Pointer to the SDL_vimStaticRegs structure to hold the static register values The static register set is defined to be the list of registers that hardware does not update by itself
Returns
0 = success -1 = failure (could not read back the static registers)