![]() |
SDL API Guide for J721E
|
Header file contains enumerations, structure definitions and function declarations for SDL EXCEPTION interface.
The SDL exception data structures include:
The SDL exception APIs include:
Go to the source code of this file.
Data Structures | |
struct | SDL_EXCEPTION_CallbackFunctions_t |
Structure of call back functions for various exception events. More... | |
Typedefs | |
typedef void(* | SDL_EXCEPTION_ECCCallback_t) (uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup) |
Format of Call back function for ECC error events. More... | |
typedef void(* | SDL_EXCEPTION_Callback_t) (void) |
Format of Call back function for exception. More... | |
Functions | |
void | SDL_EXCEPTION_init (const SDL_EXCEPTION_CallbackFunctions_t *callbackFunctions) |
Initialise Exception module. More... | |
void | SDL_EXCEPTION_registerECCHandler (SDL_EXCEPTION_ECCCallback_t ECCCallBackFunctionPtr) |
Function to register ECC exception handler. More... | |
void | SDL_EXCEPTION_undefInstructionExptnHandler (void *param) |
Undefined Instruction Exception Handler. More... | |
void | SDL_EXCEPTION_swIntrExptnHandler (void *param) |
SW Interrupt Exception Handler. More... | |
void | SDL_EXCEPTION_prefetchAbortExptnHandler (void *param) |
Prefetch Abort Exception Handler. More... | |
void | SDL_EXCEPTION_dataAbortExptnHandler (void *param) |
Data Abort Exception Handler. More... | |
void | SDL_EXCEPTION_irqExptnHandler (void *param) |
IRQ Exception Handler. More... | |
void | SDL_EXCEPTION_fiqExptnHandler (void *param) |
FIQ Exception Handler. More... | |