![]() |
SDL API Guide for J721E
|
Go to the source code of this file.
Functions | |
void | SDL_ECC_UTILS_enableECCATCM (void) |
void | SDL_ECC_UTILS_enableECCB0TCM (void) |
void | SDL_ECC_UTILS_enableECCB1TCM (void) |
void | SDL_ECC_UTILS_configSecIntr (uint32_t eventCountInitValue, uint32_t eventTypeBitMap, uint32_t counterNumber) |
void SDL_ECC_UTILS_enableECCATCM | ( | void | ) |
void SDL_ECC_UTILS_enableECCB0TCM | ( | void | ) |
void SDL_ECC_UTILS_enableECCB1TCM | ( | void | ) |
void SDL_ECC_UTILS_configSecIntr | ( | uint32_t | eventCountInitValue, |
uint32_t | eventTypeBitMap, | ||
uint32_t | counterNumber | ||
) |