![]() |
SDL API Guide for J721E
|
Enumerations | |
enum | SDL_MCRC_InstType { NAVSS0_MCRC_0 = 1, MCRC_MCU_NAVSS = 2, SDL_MCRC_INVALID = 0xffff } |
MCRC Instance supported. More... | |
enum | SDL_MCRC_dataBitSize { SDL_MCRC_DATA_8_BIT = 1U, SDL_MCRC_DATA_16_BIT = 2U, SDL_MCRC_DATA_32_BIT = 3U, SDL_MCRC_DATA_64_BIT = 4U } |
This enumerator defines the Data size for input MCRC DATA. More... | |
MCRC Operation Mode | |
typedef uint32_t | SDL_MCRC_ModeType |
MCRC operation mode supported. MCRC can either operate in Semi-CPU, Full-CPU or Auto mode. More... | |
#define | SDL_MCRC_OPERATION_MODE_DATA (SDL_MCRC_CTRL2_CH1_MODE_DATA) |
#define | SDL_MCRC_OPERATION_MODE_AUTO (SDL_MCRC_CTRL2_CH1_MODE_AUTO) |
#define | SDL_MCRC_OPERATION_MODE_SEMICPU (SDL_MCRC_CTRL2_CH1_MODE_SEMICPU) |
#define | SDL_MCRC_OPERATION_MODE_FULLCPU (SDL_MCRC_CTRL2_CH1_MODE_FULLCPU) |
MCRC channel | |
typedef uint32_t | SDL_MCRC_channel_t |
MCRC channel supported. More... | |
#define | SDL_MCRC_CHANNEL_1 (0x1U) |
#define | SDL_MCRC_CHANNEL_2 (0x2U) |
#define | SDL_MCRC_CHANNEL_3 (0x3U) |
#define | SDL_MCRC_CHANNEL_4 (0x4U) |
#define SDL_MCRC_OPERATION_MODE_DATA (SDL_MCRC_CTRL2_CH1_MODE_DATA) |
Configure MCRC operation mode to Data Captures
#define SDL_MCRC_OPERATION_MODE_AUTO (SDL_MCRC_CTRL2_CH1_MODE_AUTO) |
Configure MCRC operation mode to Auto
#define SDL_MCRC_OPERATION_MODE_SEMICPU (SDL_MCRC_CTRL2_CH1_MODE_SEMICPU) |
Configure MCRC operation mode to Semi-CPU
#define SDL_MCRC_OPERATION_MODE_FULLCPU (SDL_MCRC_CTRL2_CH1_MODE_FULLCPU) |
Configure MCRC operation mode to Full-CPU
#define SDL_MCRC_CHANNEL_1 (0x1U) |
Select channel 1 for operation
#define SDL_MCRC_CHANNEL_2 (0x2U) |
Select channel 2 for operation
#define SDL_MCRC_CHANNEL_3 (0x3U) |
Select channel 3 for operation
#define SDL_MCRC_CHANNEL_4 (0x4U) |
Select channel 4 for operation
typedef uint32_t SDL_MCRC_ModeType |
MCRC operation mode supported. MCRC can either operate in Semi-CPU, Full-CPU or Auto mode.
typedef uint32_t SDL_MCRC_channel_t |
MCRC channel supported.
enum SDL_MCRC_InstType |
enum SDL_MCRC_dataBitSize |