SDL API Guide for J721E
POK Low-Level API

Introduction

Provides the APIs for POK.

Sub Modules

 POK Data Structures
 
 POK Enum Data defines
 
 POK Functions
 

Files

file  sdl_pok_def.h
 Header file containing various enumerations, structure definitions and function declarations for the Power System modules such as POK/POR IP.
 

Functions

void sdlGetErrSig (uint32_t id, SDL_POK_Inst *instance, uint32_t *esm_err_sig, bool *usePorCfgFlag)
 

Function Documentation

◆ sdlGetErrSig()

void sdlGetErrSig ( uint32_t  id,
SDL_POK_Inst *  instance,
uint32_t *  esm_err_sig,
bool *  usePorCfgFlag 
)