SDL API Guide for J721E

Introduction

Functions

int32_t SDL_ESM_getNErrorStatus (SDL_ESM_Inst instance, uint32_t *pStatus)
 SDL ESM API to get the status of the nError pin for the specified ESM instance. More...
 
int32_t SDL_ESM_getStaticRegisters (SDL_ESM_Inst instance, SDL_ESM_staticRegs *pStaticRegs)
 SDL ESM API to read the static registers. The API reads and returns the static register configuration for the ESM module for the specified instance. This API can be used by the application to read back the static configuration. Comparision of the static configuration registers against expected values is the responsibility of the application. More...
 
int32_t SDL_ESM_verifyConfig (SDL_ESM_Inst instance, const SDL_ESM_config *pConfig)
 SDL ESM API to verify the written configuration of the ESM module. The API verifies the written config that was done during SDL_ESM_init against the provided configuration. More...
 
int32_t SDL_ESM_clrNError (SDL_ESM_Inst instance)
 SDL ESM API to clear the nError pin for the specified ESM instance. More...
 
int32_t SDL_ESM_setNError (SDL_ESM_Inst instance)
 SDL ESM API to set the nError pin for the specified ESM instance. More...
 
int32_t SDL_ESM_registerECCCallback (SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback eccCallback, void *callbackArg)
 There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The ECC module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application. More...
 
int32_t SDL_ESM_registerCCMCallback (SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback ccmCallback, void *callbackArg)
 There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The CCM module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application. More...
 
int32_t SDL_ESM_init (SDL_ESM_Inst instance, const SDL_ESM_config *pConfig, SDL_ESM_applicationCallback applicationCallback, void *appArg)
 SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the provided configuration. The configuration will allow the application to specify for each event whether the interrupt is enabled or disabled, the priority of the event, and whether the nErrorPin assertion is enabled or disabled for the event. More...
 

Function Documentation

◆ SDL_ESM_getNErrorStatus()

int32_t SDL_ESM_getNErrorStatus ( SDL_ESM_Inst  instance,
uint32_t *  pStatus 
)

SDL ESM API to get the status of the nError pin for the specified ESM instance.

Parameters
instanceESM Instance
pStatusPointer to variable to store the status. If status is 1, then error pin is not active. If status is 0, then error pin is active.
Returns
SDL_PASS if nError pin status is successfully retrieved. SDL_EBADARGS if instance or pStatus pointer are invalid. SDL_EFAIL if fail to read the error pin.

◆ SDL_ESM_getStaticRegisters()

int32_t SDL_ESM_getStaticRegisters ( SDL_ESM_Inst  instance,
SDL_ESM_staticRegs pStaticRegs 
)

SDL ESM API to read the static registers. The API reads and returns the static register configuration for the ESM module for the specified instance. This API can be used by the application to read back the static configuration. Comparision of the static configuration registers against expected values is the responsibility of the application.

Parameters
instanceESM Instance
pStaticRegsPointer to the static config register structure
Returns
SDL_PASS if registers are successfully read. SDL_EBADARGS if instance or pStaticRegs are invalid.

◆ SDL_ESM_verifyConfig()

int32_t SDL_ESM_verifyConfig ( SDL_ESM_Inst  instance,
const SDL_ESM_config pConfig 
)

SDL ESM API to verify the written configuration of the ESM module. The API verifies the written config that was done during SDL_ESM_init against the provided configuration.

Parameters
instanceESM Instance
pConfigPointer to the ESM configuration to be used for verification.
Returns
SDL_PASS if Verification passed SDL_EBADARGS if instance or pConfig are invalid. SDL_EFAIL if verification failed.

◆ SDL_ESM_clrNError()

int32_t SDL_ESM_clrNError ( SDL_ESM_Inst  instance)

SDL ESM API to clear the nError pin for the specified ESM instance.

Parameters
instanceESM Instance
Returns
SDL_PASS if nError pin status is successfully cleared. SDL_EBADARGS if instance is invalid.

◆ SDL_ESM_setNError()

int32_t SDL_ESM_setNError ( SDL_ESM_Inst  instance)

SDL ESM API to set the nError pin for the specified ESM instance.

Parameters
instanceESM Instance
Returns
SDL_PASS if nError pin status is successfully set. SDL_EBADARGS if instance is invalid.

◆ SDL_ESM_registerECCCallback()

int32_t SDL_ESM_registerECCCallback ( SDL_ESM_Inst  instance,
uint32_t  eventBitMap[],
SDL_ESM_applicationCallback  eccCallback,
void *  callbackArg 
)

There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The ECC module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application.

Parameters
instanceESM Instance
eventBitMapBitmap for ESM error event of interest for this callback. Array of uint32_t type with each bit representing one ESM error event.
eccCallbackPointer to the callback to be called by the ESM Handler to notify the ECC module of an ESM error event
callbackArgArgument that will be passed along with the callback.
Returns
SDL_PASS if success. SDL_EBADARGS if invalid argument is passed. SDL_EFAIL if other failure.

◆ SDL_ESM_registerCCMCallback()

int32_t SDL_ESM_registerCCMCallback ( SDL_ESM_Inst  instance,
uint32_t  eventBitMap[],
SDL_ESM_applicationCallback  ccmCallback,
void *  callbackArg 
)

There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The CCM module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application.

Parameters
instanceESM Instance
eventBitMapBitmap for ESM error event of interest for this callback. Array of uint32_t type with each bit representing one ESM error event.
ccmCallbackPointer to the callback to be called by the ESM Handler to notify the CCM module of an ESM error event
callbackArgArgument that will be passed along with the callback.
Returns
SDL_PASS if success. SDL_EBADARGS if invalid argument is passed. SDL_EFAIL if other failure.

◆ SDL_ESM_init()

int32_t SDL_ESM_init ( SDL_ESM_Inst  instance,
const SDL_ESM_config pConfig,
SDL_ESM_applicationCallback  applicationCallback,
void *  appArg 
)

SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the provided configuration. The configuration will allow the application to specify for each event whether the interrupt is enabled or disabled, the priority of the event, and whether the nErrorPin assertion is enabled or disabled for the event.

Parameters
instanceESM Instance
pConfigPointer to the ESM configuration structure
applicationCallbackPointer to the callback to be called by the ESM Handler to notify the application of an ESM error event.
appArgApplication argument that will passed to the application when the application callback is called.
Returns
SDL_PASS if success. SDL_EBADARGS if invalid argument is passed. SDL_EFAIL if other failure.