PDK API Guide for J721E
|
UDMA ring parameters.
Data Fields | |
void * | ringMem |
uint32_t | ringMemSize |
uint8_t | mode |
uint16_t | virtId |
uint32_t | elemCnt |
uint8_t | elemSize |
uint8_t | orderId |
uint8_t | asel |
uint32_t | mappedRingGrp |
uint32_t | mappedChNum |
void* Udma_RingPrms::ringMem |
Pointer to ring memory. Incase of FQ and CQ rings, this cannot be NULL except for DRU direct TR mode where the rings are not used. Incase of TD CQ, this can be NULL when TD response is supressed via supressTdCqPkt channel parameter. Note: This is a virtual pointer.
uint32_t Udma_RingPrms::ringMemSize |
Size of the memory in bytes allocated. This is used by the driver to validate the allocated memory is sufficient or not.
Note: By default this parameter will be set to UDMA_RING_SIZE_CHECK_SKIP by UdmaRingPrms_init API to enable backward combatibility when this is not set rightly by the caller
uint8_t Udma_RingPrms::mode |
Ring mode. Refer tisci_msg_rm_ring_cfg_req::mode
uint16_t Udma_RingPrms::virtId |
Ring virt ID. Refer tisci_msg_rm_ring_cfg_req::virtid
uint32_t Udma_RingPrms::elemCnt |
Ring element count. Set to queue depth of the ring. Set to 0 for DRU direct TR mode.
uint8_t Udma_RingPrms::elemSize |
Ring element size. Refer Udma_RingElemSize for supported values.
uint8_t Udma_RingPrms::orderId |
Ring bus order ID value to be programmed into the orderid field of the ring's RING_ORDERID register.
uint8_t Udma_RingPrms::asel |
Ring ASEL (address select) value to be set into the ASEL field of the ring's RING_BA_HI register. Refer Udma_RingAccAselEndpointSoc for supported values. This field is not supported on some SoCs.
On SoCs that do not support this field the input is quietly ignored. Note: By default this parameter will be set to UDMA_RINGACC_ASEL_ENDPOINT_PHYSADDR by UdmaRingPrms_init API
uint32_t Udma_RingPrms::mappedRingGrp |
The Mapped ring group to use when channel type is UDMA_CH_TYPE_TX_MAPPED or UDMA_CH_TYPE_RX_MAPPED.
Refer Udma_MappedTxGrpSoc macro for details about mapped TX ring groups or Udma_MappedRxGrpSoc macro for details about mapped RX ring groups.
For unmapped case, set to UDMA_MAPPED_GROUP_INVALID
uint32_t Udma_RingPrms::mappedChNum |
The assigned mapped channel number when channel type is UDMA_CH_TYPE_TX_MAPPED or UDMA_CH_TYPE_RX_MAPPED.
This is used to allocate the corresponding mapped ring for the particular channel. RM will derive an intersecting pool based on the rings reserved for the core (in rmcfg) and the permissible range for the given channel(rings reserved for specific channels) such that the allocated ring will be from this intersecting pool.
For example, If the rings idx reserved for the core are 10 to 20 and the rings for the channel are 15 to 25. Then the intersecting pool of ring idx will be 15 - 20 and rm will allocate from this range.