PDK API Guide for J721E
|
Host port module configuration parameters.
Data Fields | |
Enet_CrcType | crcType |
bool | removeCrc |
bool | padShortPacket |
bool | passCrcErrors |
uint32_t | rxMtu |
bool | passPriorityTaggedUnchanged |
bool | csumOffloadEn |
bool | rxVlanRemapEn |
bool | rxDscpIPv4RemapEn |
bool | rxDscpIPv6RemapEn |
EnetPort_VlanCfg | vlanCfg |
EnetHostPort_IngressPriorityType | rxPriorityType |
EnetPort_EgressPriorityType | txPriorityType |
Enet_CrcType CpswHostPort_Cfg::crcType |
Type of CRC on all port 0 egress, regardless of the CRC type in Ethernet port ingress
bool CpswHostPort_Cfg::removeCrc |
Whether or not CRC is removed on port 0 egress
bool CpswHostPort_Cfg::padShortPacket |
Whether short packets (ingress) are padded to 64-bytes or dropped
bool CpswHostPort_Cfg::passCrcErrors |
Whether packets with CRC errors (ingress) are dropped or transferred to the destination ports
uint32_t CpswHostPort_Cfg::rxMtu |
Max length of a received frame on ingress, including VLAN
bool CpswHostPort_Cfg::passPriorityTaggedUnchanged |
Whether priority tagged packets should be passed unchanged (if set to BTRUE) or replaced with port's VID (if set to BFALSE)
bool CpswHostPort_Cfg::csumOffloadEn |
Enable checksum offload feature which allows TCP checksum computation to be offloaded to the CPSW for frames transmitted by any core. The Protocol specific info needs to be populated in the descriptor to indicate the location in the packet where the computed checksum should be inserted
bool CpswHostPort_Cfg::rxVlanRemapEn |
RX VLAN remap controls whether the hardware switch priority for VLAN tagged or priority tagged packets is determined from CPPI thread number (remap disabled) or via ENET_HOSTPORT_IOCTL_SET_PRI_REGEN_MAP (remap enabled)
bool CpswHostPort_Cfg::rxDscpIPv4RemapEn |
RX DSCP IPv4 remap controls whether the hardware switch priority for IPv4 packets is determined from CPPI thread number (remap disabled) or via ENET_HOSTPORT_IOCTL_SET_INGRESS_DSCP_PRI_MAP (remap enabled)
bool CpswHostPort_Cfg::rxDscpIPv6RemapEn |
RX DSCP IPv6 remap controls whether the hardware switch priority for IPv6 packets is determined from CPPI thread number (remap disabled) or via ENET_HOSTPORT_IOCTL_SET_INGRESS_DSCP_PRI_MAP (remap enabled)
EnetPort_VlanCfg CpswHostPort_Cfg::vlanCfg |
Port VLAN configuration
EnetHostPort_IngressPriorityType CpswHostPort_Cfg::rxPriorityType |
Ingress priority type
EnetPort_EgressPriorityType CpswHostPort_Cfg::txPriorityType |
Egress priority type