PDK API Guide for J721E
|
ClockP interface
Files | |
file | ClockP.h |
Clock module for the RTOS Porting Interface. This implements the software timer support. For hardware timer support, please check TimerP.h. | |
Data Structures | |
struct | ClockP_Params |
Basic ClockP Parameters. More... | |
Functions | |
void | ClockP_Params_init (ClockP_Params *params) |
Initialize params structure to default values. More... | |
ClockP_Handle | ClockP_create (ClockP_FxnCallback clockfxn, const ClockP_Params *params) |
Function to create a clock. More... | |
ClockP_Status | ClockP_delete (ClockP_Handle handle) |
Function to delete a clock. More... | |
ClockP_Status | ClockP_start (ClockP_Handle handle) |
Function to start a clock. More... | |
ClockP_Status | ClockP_stop (ClockP_Handle handle) |
Function to stop a clock. More... | |
Typedefs | |
typedef void * | ClockP_Handle |
Opaque client reference to an instance of a ClockP. More... | |
typedef void(* | ClockP_FxnCallback) (void *args) |
Callback that is called when the clock expires. More... | |
Status codes for ClockP APIs | |
typedef int32_t | ClockP_Status |
Status codes for ClockP APIs. More... | |
#define | ClockP_OK ((int32_t) 0) |
#define | ClockP_FAILURE ((int32_t) (-1)) |
Timer runtime modes for ClockP APIs | |
typedef uint8_t | ClockP_RunMode |
This enumerator defines the Timer runtime modes. More... | |
#define | ClockP_RunMode_ONESHOT ((uint8_t) 0U) |
#define | ClockP_RunMode_CONTINUOUS ((uint8_t) 1U) |
Timer start modes for ClockP APIs | |
typedef uint8_t | ClockP_StartMode |
This enumerator defines the Timer start modes. More... | |
#define | ClockP_StartMode_USER ((uint8_t) 0U) |
#define | ClockP_StartMode_AUTO ((uint8_t) 1U) |
#define ClockP_OK ((int32_t) 0) |
API completed successfully
#define ClockP_FAILURE ((int32_t) (-1)) |
API failed
#define ClockP_RunMode_ONESHOT ((uint8_t) 0U) |
Timer runs for a single period values and stops
#define ClockP_RunMode_CONTINUOUS ((uint8_t) 1U) |
Timer is periodic and runs continuously
#define ClockP_StartMode_USER ((uint8_t) 0U) |
Timer will be started by the user
#define ClockP_StartMode_AUTO ((uint8_t) 1U) |
Timer starts automatically after create or scheduler start
typedef int32_t ClockP_Status |
Status codes for ClockP APIs.
typedef uint8_t ClockP_RunMode |
This enumerator defines the Timer runtime modes.
typedef uint8_t ClockP_StartMode |
This enumerator defines the Timer start modes.
typedef void* ClockP_Handle |
Opaque client reference to an instance of a ClockP.
A ClockP_Handle returned from the ClockP_create represents that instance and is used in the other instance based functions
typedef void(* ClockP_FxnCallback) (void *args) |
Callback that is called when the clock expires.
args | [in] user specific argument pointer that was passed via ClockP_Params |
void ClockP_Params_init | ( | ClockP_Params * | params | ) |
Initialize params structure to default values.
params | Pointer to the instance configuration parameters. |
ClockP_Handle ClockP_create | ( | ClockP_FxnCallback | clockfxn, |
const ClockP_Params * | params | ||
) |
Function to create a clock.
clockfxn | Function pointer of the clock function ClockP_FxnCallback. |
params | Pointer to the instance configuration parameters. |
ClockP_Status ClockP_delete | ( | ClockP_Handle | handle | ) |
Function to delete a clock.
handle | A ClockP_Handle returned from ClockP_create |
ClockP_Status ClockP_start | ( | ClockP_Handle | handle | ) |
Function to start a clock.
handle | A ClockP_Handle returned from ClockP_create |
ClockP_Status ClockP_stop | ( | ClockP_Handle | handle | ) |
Function to stop a clock.
handle | A ClockP_Handle returned from ClockP_create |