![]() |
MCUSW
|
Structure for enumerating the clock outputs of HSDIVIDER.
Data Fields | |
| uint16 | N |
| uint16 | M2 |
| uint16 | FracM |
| uint16 | sdDiv |
| uint64 | MCU_PLL_CLKOUT |
| uint64 | MCU_PLL_HSDIV0 |
| uint64 | MCU_PLL_HSDIV1 |
| uint64 | MCU_PLL_HSDIV2 |
| uint64 | MCU_PLL_HSDIV3 |
| uint16 Mcu_PllClkDivType::N |
| uint16 Mcu_PllClkDivType::M2 |
| uint16 Mcu_PllClkDivType::FracM |
| uint16 Mcu_PllClkDivType::sdDiv |
| uint64 Mcu_PllClkDivType::MCU_PLL_CLKOUT |
| uint64 Mcu_PllClkDivType::MCU_PLL_HSDIV0 |
| uint64 Mcu_PllClkDivType::MCU_PLL_HSDIV1 |
| uint64 Mcu_PllClkDivType::MCU_PLL_HSDIV2 |
| uint64 Mcu_PllClkDivType::MCU_PLL_HSDIV3 |