MCUSW
Cdd_IpcCfg.h File Reference

Introduction

This file contains generated pre compile configurations for CDD IPC MCAL driver.

Go to the source code of this file.

Macros

#define CDD_IPC_PRE_COMPILE_VARIANT   (STD_ON)
 Pre-Compile Build Variant flag. STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild. More...
 
#define CDD_IPC_NEW_MSG_NTFY_FXN   Cdd_IpcNewMessageNotify
 
#define CDD_IPC_NEW_CTRL_MSG_NTFY_FXN   Cdd_IpcNewCtrlMessageNotify
 
CDD Driver ISR category level

Defines for CDD Driver ISR ISR category level

#define CDD_IPC_ISR_VOID   (0x00U)
 void ISR type More...
 
#define CDD_IPC_ISR_CAT1   (0x01U)
 Category 1 ISR type. More...
 
#define CDD_IPC_ISR_CAT2   (0x02U)
 Category 2 ISR type. More...
 
#define CDD_IPC_DEV_ERROR_DETECT   (STD_ON)
 Enable/disable CDD Ipc dev detect error. More...
 
#define CDD_IPC_ISR_TYPE   (CDD_IPC_ISR_CAT1)
 ISR type. More...
 
Pre-Compile Switches for API Services
#define CDD_IPC_VERSION_INFO_API   (STD_ON)
 Enable/disable version info API. More...
 
#define CDD_IPC_DEINIT_API   (STD_ON)
 Enable/disable De Initialization API. More...
 
#define CDD_IPC_ANNOUNCE_API   (STD_ON)
 Enable/disable Service Announcement API. More...
 
#define CDD_IPC_REGISTER_READBACK_API   (STD_ON)
 Enable/disable Critical Register read back API. More...
 
#define CDD_IPC_SAFETY_DIAGNOSTIC_API   (STD_ON)
 Enable/disable safety diagnostics API. More...
 
#define CDD_IPC_IS_INIT_DONE_API   (STD_ON)
 Enable/disable Cdd_IpcIsInitDone API. More...
 
#define CDD_IPC_GET_MAX_MSG_SIZE_API   (STD_ON)
 Enable/disable Cdd_IpcGetMaxMsgSize API. More...
 
Dependency configurations
#define CDD_IPC_OS_COUNTER_ID   ((CounterType)OsCounter_0)
 Counter ID for counter used to count wait ticks. More...
 
Cdd Ipc DEM Error codes to report

Pre-compile switches for enabling/disabling DEM events

#define CDD_IPC_E_HARDWARE_ERROR   (DemConf_DemEventParameter_CDD_IPC_E_HARDWARE_ERROR)
 Hardware failed. More...
 
CORE Names
#define CDD_IPC_CORE_MCU1_0   (1U)
 
#define CDD_IPC_CORE_MCU1_1   (2U)
 
#define CDD_IPC_CORE_MCU2_0   (3U)
 
#define CDD_IPC_CORE_MCU2_1   (4U)
 
#define CDD_IPC_CORE_MCU3_0   (5U)
 
#define CDD_IPC_CORE_MCU3_1   (6U)
 
#define CDD_IPC_CORE_C66X_1   (7U)
 
#define CDD_IPC_CORE_C66X_2   (8U)
 
#define CDD_IPC_CORE_C7X_1   (9U)
 
#define CDD_IPC_CORE_MAX_PROCS   (11U)
 
#define CDD_IPC_OWN_CORE_ID   (CDD_IPC_CORE_MCU1_0)
 Used core identifiers. More...
 
#define CDD_IPC_REMOTE_CORE_MCU2_0_USED
 
VirtIO Object
#define CDD_IPC_VERTIO_OBJECT_SIZE   (0x1000U)
 
Communication Channel ID & Configured Buffer sizes
#define CddIpcConf_IpcComChanId_Cdd_IpcMcu20   (0U)
 
#define CDD_IPC_RPMSG_OBJ_SIZE   (256U)
 
#define CDD_IPC_NUM_VRING_BUFF   (256U)
 
#define CDD_IPC_MAX_MSG_LENGTH   (512U)
 
#define CDD_IPC_CH_0_BUFF_SIZE   ((256U * (496U + 32U)) + CDD_IPC_RPMSG_OBJ_SIZE)
 
#define CDD_IPC_MAX_CHANNEL_CFG   (2U)
 
#define IPC_VRING_BUFFER_SIZE   (0x1C00000U)
 VRing Buffer Size required for all core combinations. More...
 
#define IPC_MPU1_0   (0U)
 Core definitions. More...
 
#define IPC_MCU1_0   (1U)
 
#define IPC_MCU1_1   (2U)
 
#define IPC_MCU2_0   (3U)
 
#define IPC_MCU2_1   (4U)
 
#define IPC_MCU3_0   (5U)
 
#define IPC_MCU3_1   (6U)
 
#define IPC_C66X_1   (7U)
 
#define IPC_C66X_2   (8U)
 
#define IPC_C7X_1   (9U)
 
#define IPC_MPU1_1   (10U)
 
#define IPC_MAX_PROCS   (11U)
 
#define CDD_IPC_CORE_ID_MAX   (11U)
 IPC maximum possible core ID. More...
 
#define CDD_IPC_CORE_USED   (1U)
 
#define IPC_MAILBOX_CLUSTER_CNT   (12U)
 

Functions

void Cdd_IpcNewMessageNotify (void)
 New Message notification function. More...
 
void Cdd_IpcNewCtrlMessageNotify (uint32 remoteProcId)
 New Control Message notification function. More...
 
void Cdd_IpcIrqMbxFromMcu_20 (void)
 A Mailbox can raise multiple interrupts. In this implementation, the Mailbox new message interrupt is used determine presence of data from the remote core in the vring. More...
 

Variables

const uint32 IPC_Mailbox_BasePhyAddr [IPC_MAILBOX_CLUSTER_CNT]
 
Ipc_ProcInfo g_Ipc_mp_procInfo [IPC_MAX_PROCS]
 Processor IDs to name mapping for all processor in Jacinto7. More...
 
Ipc_MailboxInfo g_IPC_MailboxInfo [IPC_MAX_PROCS][IPC_MAX_PROCS]
 
const struct Cdd_IpcConfigType_s CddIpcConfiguraions_PC
 
uint8 Cdd_IpcDrvVertIoObj [CDD_IPC_VERTIO_OBJECT_SIZE]
 Communication Channels configured. More...