5.26.2. JTAG Power Analysis Tool¶
5.26.2.1. Introduction¶
The JTAG power analysis tool generates a snapshot of clock management IPs for Jacinto SoCs. The generated output includes:
PLL status and settings
PSC status and settings
Clock tree
Junction Temperature (from CCS20 Debugger only)
The tool is designed to work with the Supported Debuggers.
5.26.2.2. Features¶
Generates and Prints PLLs status/settings, PSC status/settings, clock tree and SoC junction temperature for supported Supported SoCs
Saves the output of the tool in JSON format
Provides a user configuration file to selectively print the PLL and LPSC status for a subset of IPs present on the SOC, including the Power Estimation Tool IPs/modules.
5.26.2.3. Requirements¶
To generate the PLLs status/settings, PSC status/settings, and clock tree for a SoC, you need:
J721E EVM
Debugging Software (See Usage of desired debugger for specific requirements).
5.26.2.4. Installation¶
Install node dependencies
In
jtag_power_analysis_tool/runnpm ciornpm install
5.26.2.5. Usage¶
The JTAG Power Analysis Tool operates in a two-step process:
Initially, a debugger script is executed to read the MMRs (Memory-Mapped Registers) and generate a list of key-value pairs, representing the MMR addresses and their corresponding values.
The tool then utilizes this list of key-value pairs to generate comprehensive outputs, including PLL status and settings, PSC status and settings and clock tree.
The modular structure of the JTAG Power Analysis Tool allows for easy integration with any debugger. This independence from the debugger enables the tool to be used with any debugger, making it adaptable to the needs of the user.
5.26.2.5.1. Running with Code Composer Studio (CCS)¶
Please refer to JTAG Power Analysis Tool with CCS for instructions to run this tool with CCS.
5.26.2.5.2. Running with Trace32 PowerView¶
Please refer to JTAG Power Analysis Tool with Trace32 for instructions to run this tool with Trace32.
5.26.2.6. Output Formats¶
5.26.2.6.1. JSON Files¶
The output json files are saved in jtag_power_analysis_tool/output/.
Sample output file can be found in
jtag_power_analysis_tool/docs/sample_output/<soc>.
Following is a snapshot of the JSON output file for the j784s4 SoC running Sciclient test in no boot mode.
5.26.2.6.1.1. PLL¶
5.26.2.6.1.1.1. Description¶
The plls_status_<soc>.json is a JSON file that represents the PLL
clock configuration. It contains the status of each PLL in the SoC. The
file is organized as a JSON object, where each key represents a specific
PLL and the corresponding value is another JSON object that contains the
PLL status.
5.26.2.6.1.1.2. Clock Configuration Key¶
isEnable: Boolean value indicating whether the PLL is enabled.
numHsdiv: Integer value specifying the number of high-speed dividers.
freqOut: Object with foutVco and foutPostDiv properties.
hsdivOut: Array of objects with idx, isEnable, freqOut, and hsDiv properties.
settings: Object with postDiv1, postDiv2, vcoFreqMul, M, fracM, and isPostDivEn properties.
"PLLFRACF2_SSMOD_16FFT_MAIN_12": {
"isEnable": 1,
"numHsdiv": 1,
"freqOut": {
"foutVco": 2133,
"foutPostDiv": 2133
},
"hsdivOut": [
{
"idx": 0,
"isEnable": 1,
"freqOut": 1066.5,
"hsDiv": 2
}
],
"settings": {
"postDiv1": 1,
"postDiv2": 1,
"vcoFreqMul": 111.09375,
"M": 111,
"fracM": 1572864,
"isPostDivEn": 1
}
},
5.26.2.6.1.2. PSC¶
5.26.2.6.1.2.1. Description¶
The psc_status_<soc>.json is a hierarchical JSON object that
represents the status of PSC.
5.26.2.6.1.2.2. Hierarchy¶
The hierarchy is as follows:
PSC: Top-level keys representing individual PSCs (e.g. WKUP_PSC0).
PD: Each PSC contains multiple Power Domains (PDs).
LPSC: Each PD contains multiple LPSCs.
IP: Each LPSC is connected to a list of IPs.
5.26.2.6.1.2.3. Properties¶
PSC: Top-level key representing a PSC, containing multiple:
PD: An object with multiple PD properties.
PD: An object representing a Power Domain, containing multiple:
LPSC: An object with multiple LPSC properties.
LPSC: An object representing a Local Power & State Controller, containing:
status: A string indicating the status of the LPSC (ENABLED or DISABLED).
controlled_ip_instances: An array of strings representing the IPs connected to the LPSC
"WKUP_PSC0": {
"PD_wkup": {
"status": "ENABLED",
"lpsc_list": {
"LPSC_wkup_alwayson": {
"status": "ENABLED",
"controlled_ip_instances": [...]
},
...
}
},
"PD_mcu_pulsar": {
"status": "ENABLED",
"lpsc_list": {
"LPSC_mcu_r5_0": {
"status": "ENABLED",
"controlled_ip_instances": [...]
},
...
}
}
}
5.26.2.6.1.3. Clock Tree¶
The clock_tree_<soc>.json is a hierarchical JSON object. Each key in
the clock tree represents a clock IP instance. Each clock IP instance
has multiple input clocks. For each input clock, the JSON array lists
the clock and its frequency starting from the root clock.
{
"IP1":[
[{clk: "clk0", freq_mhz: 1000}, {clk: "clk1", freq_mhz: 200}, {clk: "clk2", freq_mhz: 100}],
[{clk: "clk0", freq_mhz: 1000}, {clk: "clk1", freq_mhz: 200}, {clk: "clk2", freq_mhz: 50}],
],
"IP2":[
[{clk: "clk3", freq_mhz: 2000}, {clk: "clk4", freq_mhz: 400}, {clk: "clk5", freq_mhz: 400}],
[{clk: "clk3", freq_mhz: 2000}, {clk: "clk4", freq_mhz: 500}, {clk: "clk5", freq_mhz: 250}],
]
}
For example, the J784S4_DEV_MCU_ADC12FC_16FFC0 key in J784s4
represents the clock paths for the ADC IP. The array contains three
elements(adc_clk, sys_clk, and vbus_clk), each representing a clock path.
Each path includes the clock and its frequency.
"J784S4_DEV_MCU_ADC12FC_16FFC0": [
[
{
"clk": "CLK_J784S4_GLUELOGIC_HFOSC0_CLKOUT",
"freq_mhz": 19.2
},
{
"clk": "CLK_J784S4_MCU_ADC_CLK_SEL_OUT0",
"freq_mhz": 19.2
},
{
"clk": "DEV_MCU_ADC12FC_16FFC0_ADC_CLK",
"freq_mhz": 19.2
}
],
[
{
"clk": "CLK_J784S4_GLUELOGIC_HFOSC0_CLKOUT",
"freq_mhz": 19.2
},
{
"clk": "CLK_J784S4_PLLFRACF2_SSMOD_16FFT_MCU_0_FOUTVCOP_CLK",
"freq_mhz": 2000
},
{
"clk": "CLK_J784S4_HSDIV1_16FFT_MCU_0_HSDIVOUT0_CLK",
"freq_mhz": 1000
},
{
"clk": "CLK_J784S4_K3_PLL_CTRL_WRAP_WKUP_0_SYSCLKOUT_CLK",
"freq_mhz": 1000
},
{
"clk": "CLK_J784S4_K3_PLL_CTRL_WRAP_WKUP_0_CHIP_DIV1_CLK_CLK",
"freq_mhz": 1000
},
{
"clk": "DEV_MCU_ADC12FC_16FFC0_SYS_CLK",
"freq_mhz": 500
}
],
[
{
"clk": "CLK_J784S4_GLUELOGIC_HFOSC0_CLKOUT",
"freq_mhz": 19.2
},
{
"clk": "CLK_J784S4_PLLFRACF2_SSMOD_16FFT_MCU_0_FOUTVCOP_CLK",
"freq_mhz": 2000
},
{
"clk": "CLK_J784S4_HSDIV1_16FFT_MCU_0_HSDIVOUT0_CLK",
"freq_mhz": 1000
},
{
"clk": "CLK_J784S4_K3_PLL_CTRL_WRAP_WKUP_0_SYSCLKOUT_CLK",
"freq_mhz": 1000
},
{
"clk": "CLK_J784S4_K3_PLL_CTRL_WRAP_WKUP_0_CHIP_DIV1_CLK_CLK",
"freq_mhz": 1000
},
{
"clk": "DEV_MCU_ADC12FC_16FFC0_VBUS_CLK",
"freq_mhz": 333.3333
}
]
],
5.26.2.6.2. Junction Temperature¶
This JSON file contains junction temperature data for the SoC. Each object in the list represents the temperature measured by a sensor located at the specified core and vddDomain.
tempMiliDegC- The temperature in millidegrees Celsius.description- A brief description of the location of the sensor in the SoC.
5.26.2.6.3. Console output¶
Print levels determine the verbosity of the output.
0- Minimal output. Only the most essential information is printed (default).1- Intermediate output. Some additional information is printed.2- Full output. All available information is printed.
Below are the trimmed-down prints available at different print levels for j784s4 SoC.
5.26.2.6.3.1. PLL¶
5.26.2.6.3.1.1. Print Level 0¶
+--------------------------------------------+
| PLL Configuration Table |
+------------+------------+------------------+
| Name | PLL Status | VCO Freq(MHz) |
+------------+------------+------------------+
| main_0 | ENABLED | 2000.00 |
+------------+------------+------------------+
5.26.2.6.3.1.2. Print Level 1¶
+---------------------------------------------------------------------------------------+
| PLL Configuration Table |
+------------+------------+------------------+----------+------------+------------------+
| Name | PLL Status | VCO Freq(MHz) | HSDIV | Status | Output Freq(MHz) |
+------------+------------+------------------+----------+------------+------------------+
| main_0 | ENABLED | 2000.00 | HSDIV0 | ENABLED | 500.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV1 | ENABLED | 400.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV2 | ENABLED | 200.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV3 | ENABLED | 133.33 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV4 | ENABLED | 80.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV5 | ENABLED | 50.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV6 | ENABLED | 200.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV7 | ENABLED | 200.00 |
+------------+------------+------------------+----------+------------+------------------+
| | | | HSDIV8 | ENABLED | 250.00 |
+------------+------------+------------------+----------+------------+------------------+
5.26.2.6.3.1.3. Print Level 2¶
+------------------------------------------------------------------------------------------------------------------------------------------------+
| PLL Configuration Table |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| Name | PLL Status | Config | PostDiv | VCO Freq(MHz) | Num of HSDIVs | HSDIV | Status | Output Freq(MHz) |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| main_0 | ENABLED | M=104, FracM=2796203 | ENABLED, M2=2 | 2000.00 | 9 | HSDIV0 | ENABLED | 500.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV1 | ENABLED | 400.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV2 | ENABLED | 200.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV3 | ENABLED | 133.33 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV4 | ENABLED | 80.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV5 | ENABLED | 50.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV6 | ENABLED | 200.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV7 | ENABLED | 200.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
| | | | | | | HSDIV8 | ENABLED | 250.00 |
+------------+------------+------------------------+------------------+---------------+---------------+----------+------------+------------------+
5.26.2.6.3.2. PSC¶
5.26.2.6.3.2.1. Print Level 0¶
+--------------------------------------------+
| PSC Configuration Table |
+------------+------------------+------------+
| PSC Name | PD Name | PD Status |
+------------+------------------+------------+
| WKUP_PSC0 | PD_wkup | ENABLED |
+------------+------------------+------------+
| | PD_mcu_pulsar | ENABLED |
+------------+------------------+------------+
5.26.2.6.3.2.2. Print Level 1¶
+-----------------------------------------------------------------------------------+
| PSC Configuration Table |
+------------+------------------+------------+------------------------+-------------+
| PSC Name | PD Name | PD Status | LPSC Name | LPSC Status |
+------------+------------------+------------+------------------------+-------------+
| WKUP_PSC0 | PD_wkup | ENABLED | LPSC_wkup_alwayson | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_dmsc | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_debug2dmsc | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_wkup_gpio | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_wkupmcu2main | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_main2wkupmcu | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_test | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_debug | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_mcan_0 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_mcan_1 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_ospi_0 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_ospi_1 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_hyperbus | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_i3c_0 | DISABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_i3c_1 | DISABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_adc_0 | DISABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_adc_1 | DISABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_wkup_spare0 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_wkup_spare1 | DISABLED |
+------------+------------------+------------+------------------------+-------------+
| | PD_mcu_pulsar | ENABLED | LPSC_mcu_r5_0 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_r5_1 | ENABLED |
+------------+------------------+------------+------------------------+-------------+
| | | | LPSC_mcu_pulsar_pbist_ | ENABLED |
| | | | 0 | |
+------------+------------------+------------+------------------------+-------------+
5.26.2.6.3.2.3. Print Level 2¶
+------------------------------------------------------------------------------------------------------------------------+
| PSC Configuration Table |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| PSC Name | PD Name | PD Status | LPSC Name | LPSC Status | Controlled IP Instances |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| WKUP_PSC0 | PD_wkup | ENABLED | LPSC_wkup_alwayson | ENABLED | MCU_CPSW0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_CPT2_AGGR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_CTRL_MMR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_DCC0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_DCC1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_DCC2 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_ESM0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_FSS0_FSAS_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_FSS0_HYPERBUS1P0_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_FSS0_OSPI_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_FSS0_OSPI_1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_I2C0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_I2C1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_MCSPI0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_MCSPI1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_MCSPI2 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_MSRAM_1MB0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_INTR_ROUTER_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_MCRC_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_MODSS |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_MODSS_ECC_AGGR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_PROXY0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_PSILCFG_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_RINGACC0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_SEC_PROXY0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_UDMAP_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_UDMASS |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_UDMASS_ECC_AGGR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_NAVSS0_UDMASS_INTA_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PDMA0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PDMA1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PDMA2 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PDMA3 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PLL0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_SA3_SS0_SA_UL_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_SEC_MMR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER2 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER3 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER4 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER5 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER6 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER7 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER8 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_TIMER9 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_UART0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_CTRL_MMR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_DDPA0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_ESM0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_GPIOMUX_INTRTR0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_VTM0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_dmsc | ENABLED | WKUP_SMS0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_debug2dmsc | ENABLED | |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_wkup_gpio | ENABLED | WKUP_GPIO0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_GPIO1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_I2C0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | WKUP_UART0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_wkupmcu2main | ENABLED | |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_main2wkupmcu | ENABLED | |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_test | ENABLED | MCU_EFUSE0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PBIST0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_PBIST1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_debug | ENABLED | |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_mcan_0 | ENABLED | MCU_MCAN0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_mcan_1 | ENABLED | MCU_MCAN1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_ospi_0 | ENABLED | MCU_FSS0_OSPI_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_ospi_1 | ENABLED | MCU_FSS0_OSPI_1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_hyperbus | ENABLED | MCU_FSS0_HYPERBUS1P0_0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_i3c_0 | DISABLED | MCU_I3C0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_i3c_1 | DISABLED | MCU_I3C1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_adc_0 | DISABLED | MCU_ADC0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_adc_1 | DISABLED | MCU_ADC1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_wkup_spare0 | ENABLED | WKUP_SMS0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_wkup_spare1 | DISABLED | |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | PD_mcu_pulsar | ENABLED | LPSC_mcu_r5_0 | ENABLED | MCU_R5FSS0_CORE0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_RTI0 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_r5_1 | ENABLED | MCU_R5FSS0_CORE1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | | | MCU_RTI1 |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
| | | | LPSC_mcu_pulsar_pbist_ | ENABLED | MCU_PBIST2 |
| | | | 0 | | |
+------------+------------------+------------+------------------------+-------------+------------------------------------+
5.26.2.6.3.3. PET¶
+---------------------------------------------------------------------------------+
| Frequency of Selected IPs |
+------------------------------+------------+------------------------+------------+
| IP Name | Freq(MHz) | LPSC | Status |
+------------------------------+------------+------------------------+------------+
| WKUP SMS 0 | 333.3333 | LPSC_dmsc | ENABLED |
+------------------------------+------------+------------------------+------------+
| MCU R5FSS 0 | 1000 | LPSC_wkup_alwayson | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN A72SS 0 | 2000 | LPSC_A72_Cluster_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN A72SS 1 | 2000 | LPSC_A72_Cluster_1 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN R5FSS 0 | 1000 | LPSC_Pulsar_0_R5_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN R5FSS 1 | 1000 | LPSC_Pulsar_1_R5_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN R5FSS 2 | 1000 | LPSC_Pulsar_2_R5_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN C71SS 0 | 1000 | LPSC_C71x_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN C71SS 1 | 1000 | LPSC_C71x_1 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN C71SS 2 | 1000 | LPSC_C66x_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| MAIN C71SS 3 | 1000 | LPSC_C66x_1 | ENABLED |
+------------------------------+------------+------------------------+------------+
| VPAC 0 | 720 | LPSC_VPAC | ENABLED |
+------------------------------+------------+------------------------+------------+
| VPAC 1 | 720 | LPSC_vpac_1 | ENABLED |
+------------------------------+------------+------------------------+------------+
| DMPAC 0 | 480 | LPSC_DMPAC | ENABLED |
+------------------------------+------------+------------------------+------------+
| Graphic Processing Unit 0 | 800 | LPSC_GPUCOM | ENABLED |
+------------------------------+------------+------------------------+------------+
| Video Encoder/Decoder 0 | 600 | LPSC_encode_1 | ENABLED |
+------------------------------+------------+------------------------+------------+
| Video Encoder/Decoder 1 | 600 | LPSC_decode_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| LPDDR4 EMIF 0 | 1066.5 | LPSC_EMIF_CFG_0 | ENABLED |
+------------------------------+------------+------------------------+------------+
| LPDDR4 EMIF 1 | 1066.5 | LPSC_EMIF_CFG_1 | ENABLED |
+------------------------------+------------+------------------------+------------+
| LPDDR4 EMIF 2 | 1066.5 | LPSC_emif_cfg_2 | ENABLED |
+------------------------------+------------+------------------------+------------+
| LPDDR4 EMIF 3 | 1066.5 | LPSC_emif_cfg_3 | ENABLED |
+------------------------------+------------+------------------------+------------+
5.26.2.6.3.4. Clock Tree¶
Device IP: J784S4_DEV_MCU_ADC12FC_16FFC0
Number of clocks: 3
>> GLUELOGIC_HFOSC0_CLKOUT (19.2 MHz) --> MCU_ADC_CLK_SEL_OUT0 (19.2 MHz) --> ADC12FC_16FFC0_ADC_CLK (19.2 MHz)
>> GLUELOGIC_HFOSC0_CLKOUT (19.2 MHz) --> PLLFRACF2_SSMOD_16FFT_MCU_0_FOUTVCOP_CLK (2000 MHz) --> HSDIV1_16FFT_MCU_0_HSDIVOUT0_CLK (1000 MHz) -->K3_PLL_CTRL_WRAP_WKUP_0_SYSCLKOUT_CLK (1000 MHz) --> K3_PLL_CTRL_WRAP_WKUP_0_CHIP_DIV1_CLK_CLK (1000 MHz) --> ADC12FC_16FFC0_SYS_CLK (500 MHz)
>> GLUELOGIC_HFOSC0_CLKOUT (19.2 MHz) --> PLLFRACF2_SSMOD_16FFT_MCU_0_FOUTVCOP_CLK (2000 MHz) --> HSDIV1_16FFT_MCU_0_HSDIVOUT0_CLK (1000 MHz) --> K3_PLL_CTRL_WRAP_WKUP_0_SYSCLKOUT_CLK (1000 MHz) --> K3_PLL_CTRL_WRAP_WKUP_0_CHIP_DIV1_CLK_CLK (1000 MHz) --> ADC12FC_16FFC0_VBUS_CLK (333.3333 MHz)
NOTE: Some clocks of IPs may originate from sources other than the primary HFOSC/RC, in which case the clock tree print will not display the partial path and instead say “Refer to clock architecture.”
5.26.2.7. Junction Temperature¶
+-------------------------------------------------------------------------+
| Soc Junction Temperature (C) |
+--------+---------------------------------------------+------------------+
| Sensor | Location | Temperature ( C) |
+--------+---------------------------------------------+------------------+
| 0 | Near MCU_R5FSS in VDD_MCU | 39.45 |
+--------+---------------------------------------------+------------------+
| 1 | On VDD_MCU / VDD_CPU boundary near A72 (in | 39.92 |
| | VDD_MCU) | |
+--------+---------------------------------------------+------------------+
| 2 | Near GPU in VDD_CORE | 38.98 |
+--------+---------------------------------------------+------------------+
| 3 | On VDD_CORE / VDD_CPU boundary near C7x / | 39.68 |
| | MMA (in VDD_CORE) | |
+--------+---------------------------------------------+------------------+
| 4 | On VDD_CORE / VDD_CPU boundary near A72 (in | 39.45 |
| | VDD_CORE) | |
+--------+---------------------------------------------+------------------+
| 5 | On VDD_CORE / VDD_CPU boundary near C7x / | 39.68 |
| | MMA (in VDD_CORE) | |
+--------+---------------------------------------------+------------------+
| 6 | Near LPDDR4 in VDD_CORE (DDR) | 40.61 |
+--------+---------------------------------------------+------------------+
5.26.2.8. User Config¶
To print power estimation details of specific IPs or modules, add configuration in config/.meta/<soc>/custom_ip_mapping.json. Running the tool with the –selector pet argument will then print power estimation details of the specified IP or module.
The configuration in custom_ip_mapping.json should be in the following format:
{
"MAIN R5FSS 1": {
"ip_name": "J784S4_DEV_R5FSS1_CORE0",
"input_name": "DEV_R5FSS1_CORE0_CPU_CLK",
"lpsc_name": "LPSC_Pulsar_1_R5_0"
},
"VPAC 0": {
"ip_name": "J784S4_DEV_VPAC0",
"input_name": "DEV_VPAC0_MAIN_CLK",
"lpsc_name": "LPSC_VPAC",
}
}
ip_name is the IP name, input_name is the particular clock of
that IP, and lpsc_name is the LPSC of that IP.
Refer to TISCI for IP name & TRM for LPSC name.
Refer to Custom config documentation.
Output
+-----------------------------------------------------------------------------+
| Frequency of Selected IPs |
+------------------------------+------------+--------------------+------------+
| IP Name | Freq(MHz) | LPSC | Status |
+------------------------------+------------+--------------------+------------+
| MAIN R5FSS 1 | 1000 | LPSC_Pulsar_1_R5_0 | ENABLED |
+------------------------------+------------+--------------------+------------+
| VPAC 0 | 720 | LPSC_VPAC | ENABLED |
+------------------------------+------------+--------------------+------------+
5.26.2.9. Supported SoCs¶
The tool supports the following SoCs:
j784s4
j721s2
j721e
j722s
j7200
5.26.2.10. Supported Debuggers¶
CCS20.xx and above or CCS12.xx and above
Trace32 PowerView for ARM version N.2025.01.xx or above with openOCD 0.12.0 or above
5.26.2.11. Known Issues¶
Some IPs do not have divider information in .json and hence tool reads divider as 1 (E.g. ADC)
5.26.2.12. Troubleshoot¶
This section details troubleshooting techniques for resolving issues that may arise when using the JTAG Power Analysis Tool.
Missing Memory Data Initialization
File /home/cgt/ti/jacinto/workarea/pdk/packages/ti/drv/pdm_utils/tools/jtag_power_analysis_tool/memory_values_csv/j722s does not exist Memory Data is not initialized
Solution: Ensure you’ve successfully completed Step 1 of the tool’s setup instructions. This involves creating the MMR key-value pair data and providing the correct path to the tool.
MMR Read Failed - Incorrect Selector
Memory not found 67109376 0x4000200 /home/cgt/ti/jacinto/workarea/pdk/packages/ti/drv/pdm_utils/tools/jtag_power_analysis_tool/src/drv/lpsc.js:21 throw new Error("Fatal error: MMR read failed. MMR key value data is missing."); ^ Error: Fatal error: MMR read failed. MMR key value data is missing.
Explanation: This error occurs when running the tool with a different selector than the one used during the debugger execution. For example, running the debugger with selector=”pll” and the tool with selector=”pet/psc”. The debugger needs to retrieve the required MMRs to generate outputs accurately.
Solution: Use selector=”all” in pmDataGenerator(soc=”j722s”,selector = “all”) to ensure all necessary MMR data is collected.
Missing Node Modules
Error: Cannot find module minimist
Solution: Navigate to the jtag_power_analysis_tool/ directory and run either npm ci or npm install to install the required Node.js modules.
Script Path Error
js:> pmDataProcessor(soc="j722s",selector="all") Error: pm_data_generator_ccs20: file /home/cgt/ti/pdm_utils/tools/jtag_power_analysis_tool/debugger_scripts/ccs20/pm_data_generator_ccs20.js not found, please check the path in script 0.0
Solution: Update the filePath variable within the script to the absolute path of the pm_data_generator_ccs20.js file. This will ensure the tool can locate and execute the necessary script.