9. Frequently Asked QuestionsΒΆ
- 9.1. FAQ - Common
- 9.2. FAQ - CAN
- 9.3. FAQ - FVID2
- 9.4. FAQ - C7x : Steps to switch C7x SysBIOS application from secure mode to non-secure mode
- 9.4.1. Introduction
- 9.4.2. Step 1: SysBIOS config file changes to enable boot to non-secure
- 9.4.3. Step 2: Linker command file changes
- 9.4.4. Step 3: MMU initialization to setup secure and non-secure MMU tables
- 9.4.5. Step 4: CLEC initialization to allow non-secure mode access
- 9.4.6. Step 5: Cache initialization to partition L1/L2 as cache vs RAM
- 9.4.7. Step 6: Sciclient init to use non-secure mode
- 9.4.8. Step 7: Build and run
- 9.5. FAQ - Used Resources - Interrupt
- 9.6. JACINTO UDMA Resources
- 9.7. FAQ - Supported Cores by example applications
- 9.8. FAQ - How to set the clock for a given module and clock
- 9.9. FAQ - Running Apps on secure devices
- 9.10. FAQ - CSI2RX