![]() |
PDK API Guide for J721E
|
Functions | |
| int32_t | EnetRm_open (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize) |
| Open and initialize Enet RM module. More... | |
| int32_t | EnetRm_rejoin (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId) |
| Rejoin Enet RM module for a running peripheral. More... | |
| int32_t | EnetRm_ioctl (EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms) |
| Run an IOCTL operation on Enet RM. More... | |
| void | EnetRm_close (EnetMod_Handle hMod) |
| Close Enet RM module. More... | |
Typedefs | |
| typedef EnetRm_FreeRxFlowInArgs | EnetRm_ValidateRxFlowInArgs |
| Input args for ENET_RM_IOCTL_VALIDATE_RX_FLOW command. More... | |
| typedef EnetRm_Obj * | EnetRm_Handle |
| Enet RM module handle. More... | |
Macros | |
| #define | ENET_RM_PUBLIC_IOCTL(x) |
| Helper macro to create IOCTL commands for Enet RM module. More... | |
| #define | ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX (16U) |
| Maximum number of entries for IOCTL permission. More... | |
| #define | ENET_RM_NUM_MACADDR_MAX (10U) |
| Maximum number of macaddress to be managed by RM. More... | |
| #define | ENET_RM_NUM_RXCHAN_MAX (1U) |
| Maximum number of RX channels (i.e. sets of flows) More... | |
| #define | ENET_RM_PRIVATE_IOCTL(x) |
| Helper macro to create private IOCTL commands for Enet RM module. More... | |
Resource Manager Error Codes | |
| #define | ENET_RM_TXCHNUM_INVALID (0xABCDABCDU) |
| Enet RM invalid TX channel number. More... | |
| #define | ENET_RM_RXFLOWIDX_INVALID (0xABCDABCDU) |
| Enet RM invalid RX flow id. More... | |
| #define | ENET_RM_UNDEFINED_NODEID (0xABCDABCDU) |
| Enet RM undefined node id. More... | |
| #define | ENET_RM_INVALIDCORE (0x5562AEFEU) |
| Enet RM invalid core. More... | |
| #define ENET_RM_PUBLIC_IOCTL | ( | x | ) |
Helper macro to create IOCTL commands for Enet RM module.
| #define ENET_RM_TXCHNUM_INVALID (0xABCDABCDU) |
Enet RM invalid TX channel number.
| #define ENET_RM_RXFLOWIDX_INVALID (0xABCDABCDU) |
Enet RM invalid RX flow id.
| #define ENET_RM_UNDEFINED_NODEID (0xABCDABCDU) |
Enet RM undefined node id.
| #define ENET_RM_INVALIDCORE (0x5562AEFEU) |
Enet RM invalid core.
| #define ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX (16U) |
Maximum number of entries for IOCTL permission.
| #define ENET_RM_NUM_MACADDR_MAX (10U) |
Maximum number of macaddress to be managed by RM.
| #define ENET_RM_NUM_RXCHAN_MAX (1U) |
Maximum number of RX channels (i.e. sets of flows)
| #define ENET_RM_PRIVATE_IOCTL | ( | x | ) |
Helper macro to create private IOCTL commands for Enet RM module.
Input args for ENET_RM_IOCTL_VALIDATE_RX_FLOW command.
| typedef EnetRm_Obj* EnetRm_Handle |
Enet RM module handle.
| enum EnetRm_Ioctls |
Enet RM IOCTL commands.
| Enumerator | |
|---|---|
| ENET_RM_IOCTL_ALLOC_MAC_ADDR | Alloc MAC address. IOCTL parameters:
|
| ENET_RM_IOCTL_FREE_MAC_ADDR | Free MAC address. IOCTL parameters:
|
| ENET_RM_IOCTL_ALLOC_RX_FLOW | Alloc RX flow. IOCTL parameters:
|
| ENET_RM_IOCTL_FREE_RX_FLOW | Free RX flow. IOCTL parameters:
|
| ENET_RM_IOCTL_ALLOC_TX_CH_PEERID | Alloc TX channel peer id. IOCTL parameters:
|
| ENET_RM_IOCTL_FREE_TX_CH_PEERID | Free TX channel peer id. IOCTL parameters:
|
| ENET_RM_IOCTL_ALLOC_HW_PUSH_INST | Alloc HW Push instance. IOCTL parameters:
|
| ENET_RM_IOCTL_FREE_HW_PUSH_INST | Free HW Push instance. IOCTL parameters:
|
| enum EnetRm_TxCh |
RM tx channel.
This enum holds the number of tx channel.
| enum EnetRm_NodeType |
| enum EnetRm_PrivIoctls |
Enet RM private IOCTL commands.
| Enumerator | |
|---|---|
| ENET_RM_IOCTL_VALIDATE_PERMISSION | Validate IOCTL permission. IOCTL parameters:
|
| ENET_RM_IOCTL_ATTACH | Attach core. IOCTL parameters:
|
| ENET_RM_IOCTL_DETACH | Detach core. IOCTL parameters:
|
| ENET_RM_IOCTL_INTERNAL_ALLOC_RX_FLOW | Internal RX flow allocation. IOCTL parameters:
|
| ENET_RM_IOCTL_INTERNAL_FREE_RX_FLOW | Internal RX flow free. IOCTL parameters:
|
| ENET_RM_IOCTL_VALIDATE_RX_FLOW | Validate RX flow is allocated resource and is from a attached core. IOCTL parameters:
|
| int32_t EnetRm_open | ( | EnetMod_Handle | hMod, |
| Enet_Type | enetType, | ||
| uint32_t | instId, | ||
| const void * | cfg, | ||
| uint32_t | cfgSize | ||
| ) |
Open and initialize Enet RM module.
| hMod | Enet Module handle |
| enetType | Enet Peripheral type |
| instId | Enet Peripheral instance id |
| cfg | Configuration parameters |
| cfgSize | Size of the configuration parameters |
| int32_t EnetRm_rejoin | ( | EnetMod_Handle | hMod, |
| Enet_Type | enetType, | ||
| uint32_t | instId | ||
| ) |
Rejoin Enet RM module for a running peripheral.
| hMod | Enet Module handle |
| enetType | Enet Peripheral type |
| instId | Enet Peripheral instance id |
| int32_t EnetRm_ioctl | ( | EnetMod_Handle | hMod, |
| uint32_t | cmd, | ||
| Enet_IoctlPrms * | prms | ||
| ) |
Run an IOCTL operation on Enet RM.
| hMod | Enet Module handle |
| cmd | IOCTL command Id |
| prms | IOCTL parameters |
| void EnetRm_close | ( | EnetMod_Handle | hMod | ) |
Close Enet RM module.
| hMod | Enet Module handle |