VXLIB User Guide
VXLIB_tableLookup.h
Go to the documentation of this file.
1 /******************************************************************************
2  * Copyright (C) 2023 Texas Instruments Incorporated - https://www.ti.com/
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  ******************************************************************************/
33 
34 #ifndef VXLIB_TABLELOOKUP_IXX_IXX_OXX_H_
35 #define VXLIB_TABLELOOKUP_IXX_IXX_OXX_H_
36 
37 #include "../common/VXLIB_types.h"
38 
39 #ifdef __cplusplus
40 extern "C" {
41 #endif
42 
76 typedef struct {
78  int8_t funcStyle;
80  uint32_t count;
82  uint16_t offset;
83 
85 
96 
121  VXLIB_bufParams2D_t *bufParamsIn,
122  VXLIB_bufParams2D_t *bufParamsOut,
123  VXLIB_bufParams1D_t *bufParamsLut,
124  const VXLIB_tableLookup_InitArgs *pKerInitArgs);
125 
152  const VXLIB_bufParams2D_t *bufParamsIn,
153  const VXLIB_bufParams2D_t *bufParamsOut,
154  const VXLIB_bufParams1D_t *bufParamsLut,
155  const VXLIB_tableLookup_InitArgs *pKerInitArgs);
156 
168 VXLIB_tableLookup_set(VXLIB_kernelHandle handle, void *restrict pLut);
188  const void *restrict pIn,
189  const void *restrict pOut,
190  const void *restrict pLut);
191 
227 VXLIB_tableLookup_exec(VXLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut, void *restrict pLut);
228 
254  const VXLIB_bufParams2D_t *bufParamsIn,
255  const VXLIB_bufParams2D_t *bufParamsOut,
256  const VXLIB_bufParams1D_t *bufParamsLut,
257  const VXLIB_tableLookup_InitArgs *pKerInitArgs,
258  size_t *archCycles,
259  size_t *estCycles);
260 
263 #ifdef __cplusplus
264 }
265 #endif
266 
267 #endif /* VXLIB_TABLELOOKUP_IXX_IXX_OXX_H_ */
268 /* ======================================================================== */
269 /* End of file: VXLIB_tableLookup.h */
270 /* ======================================================================== */
void * VXLIB_kernelHandle
Handle type for VXLIB operations.
Definition: VXLIB_types.h:247
VXLIB_STATUS_NAME
The enumeration of all status codes.
Definition: VXLIB_types.h:220
VXLIB_STATUS VXLIB_tableLookup_exec_checkParams(VXLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut, const void *restrict pLut)
This function checks the validity of the parameters passed to VXLIB_tableLookup_exec function....
VXLIB_STATUS VXLIB_tableLookup_init(VXLIB_kernelHandle handle, VXLIB_bufParams2D_t *bufParamsIn, VXLIB_bufParams2D_t *bufParamsOut, VXLIB_bufParams1D_t *bufParamsLut, const VXLIB_tableLookup_InitArgs *pKerInitArgs)
This function should be called before the VXLIB_tableLookup_exec function is called....
void VXLIB_tableLookup_perfEst(VXLIB_kernelHandle handle, const VXLIB_bufParams2D_t *bufParamsIn, const VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_bufParams1D_t *bufParamsLut, const VXLIB_tableLookup_InitArgs *pKerInitArgs, size_t *archCycles, size_t *estCycles)
This function estimates the archCycles and estCycles.
VXLIB_STATUS VXLIB_tableLookup_exec(VXLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut, void *restrict pLut)
This function is the main kernel compute function.
VXLIB_STATUS VXLIB_tableLookup_init_checkParams(VXLIB_kernelHandle handle, const VXLIB_bufParams2D_t *bufParamsIn, const VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_bufParams1D_t *bufParamsLut, const VXLIB_tableLookup_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to VXLIB_tableLookup_init function....
int32_t VXLIB_tableLookup_getHandleSize(VXLIB_tableLookup_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
VXLIB_STATUS VXLIB_tableLookup_set(VXLIB_kernelHandle handle, void *restrict pLut)
This function place the lookup table in suitable memory location.
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
uint32_t count
Parameter indicating size of lookup table
int8_t funcStyle
Variant of the function, refer to VXLIB_FUNCTION_STYLE
uint16_t offset
Parameter indicating index of input value = 0 in the lookup table