Go to the source code of this file.
|
| int32_t | VXLIB_accumulateImage_getHandleSize (VXLIB_accumulateImage_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| VXLIB_STATUS | VXLIB_accumulateImage_init (VXLIB_kernelHandle handle, VXLIB_bufParams2D_t *bufParamsIn, VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_accumulateImage_InitArgs *pKerInitArgs) |
| | This function should be called before the VXLIB_accumulateImage_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine. The results of these operations are stored in the handle. More...
|
| |
| VXLIB_STATUS | VXLIB_accumulateImage_init_checkParams (VXLIB_kernelHandle handle, const VXLIB_bufParams2D_t *bufParamsIn, const VXLIB_bufParams2D_t *bufParamsOut, const VXLIB_accumulateImage_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to VXLIB_accumulateImage_init function. This function is called with the same parameters as the VXLIB_accumulateImage_init, and this function must be called before the VXLIB_accumulateImage_init is called. More...
|
| |
| VXLIB_STATUS | VXLIB_accumulateImage_exec_checkParams (VXLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut) |
| | This function checks the validity of the parameters passed to VXLIB_accumulateImage_exec function. This function is called with the same parameters as the VXLIB_accumulateImage_init, and this function must be called before the VXLIB_accumulateImage_init is called. More...
|
| |
| VXLIB_STATUS | VXLIB_accumulateImage_exec (VXLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| | This function is the main kernel compute function. More...
|
| |
| void | VXLIB_accumulateImage_perfEst (VXLIB_kernelHandle handle, size_t *archCycles, size_t *estCycles) |
| |