Vision Apps User Guide
network_api.h File Reference

Introduction

Wrapper API's to use TCP/IP sockets

Go to the source code of this file.

Data Structures

struct  Network_SockObj
 

Typedefs

typedef int Bool
 

Functions

int32_t Network_open (Network_SockObj *pObj, uint32_t port)
 
int32_t Network_close (Network_SockObj *pObj, Bool closeServerSock)
 
int32_t Network_waitConnect (Network_SockObj *pObj, uint32_t timeout)
 
int32_t Network_read (Network_SockObj *pObj, uint8_t *dataBuf, uint32_t *dataSize)
 
int32_t Network_write (Network_SockObj *pObj, uint8_t *dataBuf, uint32_t dataSize)
 

Typedef Documentation

◆ Bool

typedef int Bool

Function Documentation

◆ Network_open()

int32_t Network_open ( Network_SockObj pObj,
uint32_t  port 
)

◆ Network_close()

int32_t Network_close ( Network_SockObj pObj,
Bool  closeServerSock 
)

◆ Network_waitConnect()

int32_t Network_waitConnect ( Network_SockObj pObj,
uint32_t  timeout 
)

◆ Network_read()

int32_t Network_read ( Network_SockObj pObj,
uint8_t *  dataBuf,
uint32_t *  dataSize 
)

◆ Network_write()

int32_t Network_write ( Network_SockObj pObj,
uint8_t *  dataBuf,
uint32_t  dataSize 
)