Vision Apps User Guide
HW accelerator initialization APIs (RTOS only)

Introduction

This section contains APIs for HW accelerator initialization.

Functions

int32_t appFvid2Init (void)
 Performs initializations needed for Fvid2 must be called before capture, display and other HWA init. More...
 
int32_t appCsi2RxInit (void)
 Performs initializations needed for CSI2RX driver. More...
 
int32_t appCsi2TxInit (void)
 Performs initializations needed for CSI2TX driver. More...
 
int32_t appVhwaVpacInit (uint32_t vpacInst)
 Performs initializations needed for VHWA drivers. More...
 
int32_t appVhwaDmpacInit (void)
 
int32_t appCsi2RxDeInit (void)
 Performs de-initializations needed for CSI2RX driver. More...
 
int32_t appCsi2TxDeInit (void)
 Performs de-initializations needed for CSI2TX driver. More...
 
int32_t appFvid2DeInit (void)
 Performs de-initializations needed for Fvid2. More...
 
int32_t appVhwaVpacDeInit (void)
 Performs de-initializations needed for VHWA drivers. More...
 
int32_t appVhwaDmpacDeInit (void)
 
int32_t appVhwaRemoteServiceInit ()
 Performs registration of remote service for SL2. More...
 
int32_t appVhwaRemoteServiceDeInit ()
 Performs unregistration of remote service for SL2. More...
 
int32_t appVissRemoteServiceInit ()
 Performs registration of remote service for VISS node. More...
 
int32_t appVissRemoteServiceDeInit ()
 Performs unregistration of remote service for VISS node. More...
 

Function Documentation

◆ appFvid2Init()

int32_t appFvid2Init ( void  )

Performs initializations needed for Fvid2 must be called before capture, display and other HWA init.

◆ appCsi2RxInit()

int32_t appCsi2RxInit ( void  )

Performs initializations needed for CSI2RX driver.

◆ appCsi2TxInit()

int32_t appCsi2TxInit ( void  )

Performs initializations needed for CSI2TX driver.

◆ appVhwaVpacInit()

int32_t appVhwaVpacInit ( uint32_t  vpacInst)

Performs initializations needed for VHWA drivers.

◆ appVhwaDmpacInit()

int32_t appVhwaDmpacInit ( void  )

◆ appCsi2RxDeInit()

int32_t appCsi2RxDeInit ( void  )

Performs de-initializations needed for CSI2RX driver.

◆ appCsi2TxDeInit()

int32_t appCsi2TxDeInit ( void  )

Performs de-initializations needed for CSI2TX driver.

◆ appFvid2DeInit()

int32_t appFvid2DeInit ( void  )

Performs de-initializations needed for Fvid2.

◆ appVhwaVpacDeInit()

int32_t appVhwaVpacDeInit ( void  )

Performs de-initializations needed for VHWA drivers.

◆ appVhwaDmpacDeInit()

int32_t appVhwaDmpacDeInit ( void  )

◆ appVhwaRemoteServiceInit()

int32_t appVhwaRemoteServiceInit ( )

Performs registration of remote service for SL2.

◆ appVhwaRemoteServiceDeInit()

int32_t appVhwaRemoteServiceDeInit ( )

Performs unregistration of remote service for SL2.

◆ appVissRemoteServiceInit()

int32_t appVissRemoteServiceInit ( )

Performs registration of remote service for VISS node.

◆ appVissRemoteServiceDeInit()

int32_t appVissRemoteServiceDeInit ( )

Performs unregistration of remote service for VISS node.