This section contains module APIs for the image sensor framework.
◆ APP_SENSOR_FEATURE_CFG_UC0
| #define APP_SENSOR_FEATURE_CFG_UC0 (0) |
Use case config value corresponding to ISS_SENSOR_FEATURE_CFG_UC0.
◆ APP_SENSOR_FEATURE_CFG_UC1
| #define APP_SENSOR_FEATURE_CFG_UC1 (1) |
Use case config value corresponding to ISS_SENSOR_FEATURE_CFG_UC1.
◆ APP_SENSOR_FEATURE_CFG_UC2
| #define APP_SENSOR_FEATURE_CFG_UC2 (2) |
Use case config value corresponding to ISS_SENSOR_FEATURE_CFG_UC2.
◆ app_querry_sensor()
| vx_status app_querry_sensor |
( |
SensorObj * |
sensorObj | ) |
|
Sensor module query sensor helper function.
This Sensor module query function queries the user for which sensor to use and populates sensor object parameters based on the chosen sensor; also supports automatic detection of available sensors
- Parameters
-
| [in,out] | sensorObj | Sensor Module object which contains the sensor parameters |
◆ app_init_sensor()
| vx_status app_init_sensor |
( |
SensorObj * |
sensorObj, |
|
|
char * |
objName |
|
) |
| |
Sensor module init sensor helper function.
This Sensor module init function initializes the sensor after the sensor has been queried and set using the app_querry_sensor
- Parameters
-
| [in,out] | sensorObj | Sensor Module object which contains the sensor parameters |
| [in] | objName | String of the name of this object |
◆ app_deinit_sensor()
| void app_deinit_sensor |
( |
SensorObj * |
sensorObj | ) |
|
Sensor module deinit sensor helper function.
This Sensor module deinit function deinitializes the sensor
- Parameters
-
| [in,out] | sensorObj | Sensor Module object which contains the sensor parameters |