TIOVX User Guide

Detailed Description

Internal APIs for node operations.

Data Structures

struct  tivx_node_t
 The internal representation of a node. More...
 

Functions

vx_status ownSetNodeImmTarget (vx_node node)
 Set the target for node based on immediate mode target set in context. More...
 
vx_status ownSetNodeAttributeValidRectReset (vx_node node, vx_bool is_reset)
 Set the attribute VX_NODE_VALID_RECT_RESET in node. More...
 
vx_status ownNodeKernelValidate (vx_node node, vx_meta_format meta[])
 Validate user kernel or target kernel associated with this node.
 
vx_status ownNodeKernelInit (vx_node node)
 Init user kernel or target kernel associated with this node.
 
vx_status ownNodeKernelInitKernelName (vx_node node)
 Init user kernel or target kernel name associated with this node.
 
vx_status ownNodeKernelDeinitKernelName (vx_node node)
 Deinit user kernel or target kernel name associated with this node.
 
vx_status ownNodeKernelSchedule (vx_node node, uint32_t pipeline_id)
 Schedule user kernel or target kernel associated with this node for execution.
 
vx_status ownNodeKernelDeinit (vx_node node)
 DeInit user kernel or target kernel associated with this node.
 
vx_status ownResetNodePerf (vx_node node)
 Reset node performance statistics.
 
vx_status ownUpdateNodePerf (vx_node node, uint32_t pipeline_id)
 Called by graph each time after node execution.
 
uint32_t ownNodeGetNumParameters (vx_node node)
 Return number of node parameters.
 
vx_enum ownNodeGetParameterDir (vx_node node, uint32_t prm_index)
 Get direction of a parameter.
 
vx_reference ownNodeGetParameterRef (vx_node node, uint32_t prm_index)
 Get reference associated with a parameters of a parameter.
 
vx_status ownNodeAddOutNode (vx_node node, vx_node out_node)
 Associate a output node with a given node.
 
vx_status ownNodeReplaceOutNode (vx_node node, vx_node old_out_node, vx_node new_out_node)
 Replace an output node for a given node with a new output node.
 
vx_status ownNodeAddInNode (vx_node node, vx_node out_node)
 Associate a input node with a given node.
 
vx_status ownNodeReplaceInNode (vx_node node, vx_node old_in_node, vx_node new_in_node)
 Replace an input node for a given node with a new input node.
 
uint32_t ownNodeGetNumInNodes (vx_node node)
 Get number of input nodes associated with this node.
 
uint32_t ownNodeGetNumOutNodes (vx_node node)
 Get number of output nodes associated with this node.
 
vx_status ownNodeCreateUserCallbackCommand (vx_node node, uint32_t pipeline_id)
 Create resources required to call a user callback If user callback is assigned then nothing is done.
 
vx_action ownNodeExecuteUserCallback (vx_node node)
 Call user specified callback.
 
void ownNodeClearExecuteState (vx_node node, uint32_t pipeline_id)
 clears execute status of the node
 
vx_status ownNodeUserKernelExecute (vx_node node, vx_reference prm_ref[])
 Execute user kernel.
 
vx_bool ownNodeIsPrmReplicated (vx_node node, uint32_t prm_idx)
 Is prm_idx of node replicated.
 
vx_status ownNodeSetParameter (vx_node node, vx_uint32 idx, vx_reference value)
 Set parameter at node.
 
vx_node ownNodeGetNextNode (vx_node node, vx_uint32 idx)
 Get next node at given output index.
 
vx_node ownNodeGetNextInNode (vx_node node, vx_uint32 idx)
 Get next node at given input index.
 
vx_status ownNodeRegisterEvent (vx_node node, vx_enum event_type, vx_uint32 app_value, enum tivx_queue_type_e queue_type)
 Register node completion event.
 
void ownNodeCheckAndSendCompletionEvent (const tivx_obj_desc_node_t *node_obj_desc, uint64_t timestamp)
 Send node completion event if enabled.
 
void ownNodeCheckAndSendErrorEvent (const tivx_obj_desc_node_t *node_obj_desc, uint64_t timestamp, vx_status status)
 Send node error event if node failed.
 
vx_status ownNodeAllocObjDescForPipeline (vx_node node, uint32_t pipeline_depth)
 Alloc additional node obj desc's for pipelining.
 
void ownNodeSetObjDescParamDirection (vx_node node)
 Set param direction for 0th node obj desc.
 
void ownNodeLinkObjDescForPipeline (vx_node node)
 Update in node id and out node id for node pipeline obj desc's.
 
void ownNodeLinkDataRefQueue (vx_node node, uint32_t prm_id, tivx_data_ref_queue data_ref_q)
 Link data ref q to node at parameter index 'prm_id'.
 
void ownNodeLinkArrayElement (vx_node node, uint32_t prm_id)
 Link array element to node at parameter index 'prm_id'.
 
uint32_t ownNodeGetParameterNumBuf (vx_node node, vx_uint32 idx)
 Return number of buffers to allocate at a node,index. More...
 

Function Documentation

◆ ownSetNodeImmTarget()

vx_status ownSetNodeImmTarget ( vx_node  node)

Set the target for node based on immediate mode target set in context.

Parameters
[in]nodeThe reference to the node
Returns
A vx_status_e enumeration.
Return values
VX_SUCCESSNo errors.

◆ ownSetNodeAttributeValidRectReset()

vx_status ownSetNodeAttributeValidRectReset ( vx_node  node,
vx_bool  is_reset 
)

Set the attribute VX_NODE_VALID_RECT_RESET in node.

Parameters
[in]nodeThe reference to the node
[in]is_resetThe value to set for the attribute
Returns
A vx_status_e enumeration.
Return values
VX_SUCCESSNo errors.

◆ ownNodeGetParameterNumBuf()

uint32_t ownNodeGetParameterNumBuf ( vx_node  node,
vx_uint32  idx 
)

Return number of buffers to allocate at a node,index.

Valid only for output parameters

Returns 0 is user has not made any specific choice or invalid parameter