![]() |
TIOVX User Guide
|
APIs for task operations on the host.
Data Structures | |
| struct | tivx_task |
| Typedef for a task. More... | |
| struct | tivx_task_create_params_t |
| Parameters that can be set during task creation. More... | |
Defines | |
| #define | TIVX_TASK_PRI_HIGHEST (0u) |
| Constant to define highest priority for a task. | |
| #define | TIVX_TASK_PRI_LOWEST (15u) |
| Constant to define lowest priority for a task. | |
| #define | TIVX_TASK_AFFINITY_ANY (0xFFFFu) |
| constant to indicate task affinity can be decided by OS on a SMP CPU | |
| #define | TIVX_MAX_TASK_NAME (12u) |
| Max Task Name Size. | |
Typedefs | |
| typedef void(VX_CALLBACK * | tivx_task_main_f) (void *app_var) |
| Entry point of task. More... | |
Functions | |
| void | tivxTaskSetDefaultCreateParams (tivx_task_create_params_t *params) |
| Used to set default task create parameters in parameter structure. More... | |
| vx_status | tivxTaskCreate (tivx_task *task, const tivx_task_create_params_t *params) |
| Create a task. More... | |
| vx_status | tivxTaskDelete (tivx_task *task) |
| Delete a task. More... | |
| void | tivxTaskWaitMsecs (uint32_t msec) |
| waits/sleeps for given milliseconds More... | |
| typedef void(VX_CALLBACK * tivx_task_main_f) (void *app_var) |
Entry point of task.
| target | [in] target handle |
Definition at line 111 of file tivx_task.h.
| void tivxTaskSetDefaultCreateParams | ( | tivx_task_create_params_t * | params | ) |
Used to set default task create parameters in parameter structure.
| params | [out] Params to use for task creation |
| vx_status tivxTaskCreate | ( | tivx_task * | task, |
| const tivx_task_create_params_t * | params | ||
| ) |
Create a task.
| task | [out] Pointer to task object |
| params | [in] Task create parameters |
Delete a task.
| task | [in] Pointer to task object |
| void tivxTaskWaitMsecs | ( | uint32_t | msec | ) |
waits/sleeps for given milliseconds
| msec | [in] amount of milliseconds to sleep |