![]() |
TI Autonomous Driving Algorithms (TIADALG) Library User Guide
|
This file defines the interface for Voxelization and feature computation for points pillar CNN for 3D OD on lidar data. More...
#include <stdint.h>Go to the source code of this file.
Data Structures | |
| struct | voxel_info_t |
| This structure defines the property of lidar data and its voxelization. More... | |
Functions | |
| int32_t | tiadalg_voxelization_cn (float *lidar_data, int32_t num_lidar_points, int32_t *scratch_1, int32_t *scratch_2, voxel_info_t *voxel_info, void *voxel_data, int32_t *indices, int16_t *num_points, int32_t scale_fact, int32_t out_voxel_data_type) |
| It does basic voxelization. More... | |
| int32_t | tiadalg_voxel_feature_compute_cn (void *voxel_data, int32_t *indices, int16_t *num_points, voxel_info_t *voxel_info, int32_t num_voxels, int32_t scale_fact, int32_t data_type) |
| Computes feature for voxels. More... | |
This file defines the interface for Voxelization and feature computation for points pillar CNN for 3D OD on lidar data.
| int32_t tiadalg_voxelization_cn | ( | float * | lidar_data, |
| int32_t | num_lidar_points, | ||
| int32_t * | scratch_1, | ||
| int32_t * | scratch_2, | ||
| voxel_info_t * | voxel_info, | ||
| void * | voxel_data, | ||
| int32_t * | indices, | ||
| int16_t * | num_points, | ||
| int32_t | scale_fact, | ||
| int32_t | out_voxel_data_type | ||
| ) |
It does basic voxelization.
tiadalg_voxelization
| lidar_data | [in] : Input lidar data. 4xL |
| num_lidar_points | [in] : Number of lidar points |
| scratch_1 | [in] : scratch of size num_lidar_points*sizeof(uint32_t) |
| scratch_2 | [in] : scratch of size num_lidar_points*sizeof(uint32_t) |
| voxel_info | [in] : voxel info |
| voxel_data | [out] : output buffer of size nw_max_num_voxels*max_points_per_voxel*9*sizeof(out_voxel_data_type) |
| indices | [out] : output buffer of size nw_max_num_voxels*sizeof(uint32). Indicating voxel location in birds eye view |
| num_points | [out] : output buffer of size nw_max_num_voxels*sizeof(uint16). Indicating acctual number of points in each voxel |
| scale_fact | [in] : Input lidar data is multiplied with value before usages |
| out_voxel_data_type | [out] : Output voxel data type. Not used right now. It is always float32 right now. |
| int32_t tiadalg_voxel_feature_compute_cn | ( | void * | voxel_data, |
| int32_t * | indices, | ||
| int16_t * | num_points, | ||
| voxel_info_t * | voxel_info, | ||
| int32_t | num_voxels, | ||
| int32_t | scale_fact, | ||
| int32_t | data_type | ||
| ) |
Computes feature for voxels.
tiadalg_voxel_feature_compute_cn
| voxel_data | [out] : output buffer of size nw_max_num_voxels*max_points_per_voxel*9*sizeof(out_voxel_data_type) |
| indices | [in] : output buffer of size nw_max_num_voxels*sizeof(uint32). Indicating voxel location in birds eye view |
| num_points | [in] : output buffer of size nw_max_num_voxels*sizeof(uint16). Indicating acctual number of points in each voxel |
| voxel_info | [in] : voxel info |
| num_voxels | [in] : Total number of voxels given to API |
| scale_fact | [in] : Input lidar data is multiplied with value before usages |
| data_type | [in] : Not used right now. It is flaot32 always right now |
|
|
| © Copyright 2018 Texas Instruments Incorporated. All rights reserved. |
| Document generated by doxygen 1.8.6 |