![]() |
Perception Tool Kit (PTK) API Guide
|
Grid definition.

Data Fields | |
| PTK_GridConfig | config |
| float | xInvCellSize |
| float | yInvCellSize |
| float | zInvCellSize |
| uint32_t | dataCellCount |
| uint32_t | dataOffset |
| PTK_GridMetaData | metaData |
| PTK_GridConfig PTK_Grid::config |
Configuration information describing the grid organization.
| float PTK_Grid::xInvCellSize |
1/xCellSize from config data.
| float PTK_Grid::yInvCellSize |
1/yCellSize from config data.
| float PTK_Grid::zInvCellSize |
1/zCellSize from config data.
| uint32_t PTK_Grid::dataCellCount |
Number of cells in the data array.
| uint32_t PTK_Grid::dataOffset |
Offset of the data field in bytes, relative to the struct.
| PTK_GridMetaData PTK_Grid::metaData |
Holds meta data about grid.