![]() |
Perception Tool Kit (PTK) API Guide
|
Stereo algorithm - detected obstacle parameters.

Data Fields | |
| uint8_t | maxHorizontalToSkip |
| uint8_t | minHorizontalLength |
| float | windowHeightRatioRange [2] |
| float | adaptiveTerminationPercentage |
| float | maxDisparityDifference |
| float | obsProbabilityMinDisparityToAccept |
| uint8_t PTK_Alg_StereoAlgo_detectObsParams::maxHorizontalToSkip |
Tuning parameter 1 for obstacle detection
| uint8_t PTK_Alg_StereoAlgo_detectObsParams::minHorizontalLength |
Tuning parameter 2 for obstacle detection
| float PTK_Alg_StereoAlgo_detectObsParams::windowHeightRatioRange[2] |
Tuning parameter 3 for obstacle detection
| float PTK_Alg_StereoAlgo_detectObsParams::adaptiveTerminationPercentage |
Tuning parameter 4 for obstacle detection
| float PTK_Alg_StereoAlgo_detectObsParams::maxDisparityDifference |
Tuning parameter 5 for obstacle detection Disparity with difference bigger than it is declared as new obstacle
| float PTK_Alg_StereoAlgo_detectObsParams::obsProbabilityMinDisparityToAccept |
Tuning parameter 6 for obstacle detection