![]() |
Perception Tool Kit (PTK) API Guide
|


Go to the source code of this file.
Data Structures | |
| struct | PTK_Alg_StereoAlgo_GroundEstimation_allParams |
| Stereo algorithm - all required parameters structure for ground plane estimation. More... | |
| struct | PTK_Alg_StereoAlgo_GroundEstimationObj |
| Stereo algorithm - ground plane estimation context. More... | |
Functions | |
| void | PTK_Alg_StereoAlgo_GroundEstimationSetParams (PTK_Alg_StereoAlgo_GroundEstimation_allParams *allPararms, PTK_Alg_StereoAlgo_GroundEstimationObj *cntxt) |
| Initialize ground plane estimation parameters. More... | |
| int32_t | PTK_Alg_StereoAlgo_GroundEstimationConfig (PTK_Alg_StereoAlgo_GroundEstimation_allParams *cfg, PTK_Api_MemoryReq *memReq) |
| Computes the memory requirements based on the given algorithm configuration parameters. More... | |
| PTK_AlgHandle | PTK_Alg_StereoAlgo_GroundEstimationInit (PTK_Alg_StereoAlgo_GroundEstimation_allParams *allParams, const PTK_Api_MemoryRsp *memRsp) |
| Initializes the library based on the given algorithm configuration parameters and allocated memory blocks. More... | |
| int32_t | PTK_Alg_StereoAlgo_GroundEstimationGetMem (PTK_Alg_StereoAlgo_GroundEstimationObj *cntxt, uint8_t *memPtr) |
| Get memory size. More... | |
| void | PTK_Alg_StereoAlgo_GroundEstimationReset (PTK_Alg_StereoAlgo_GroundEstimationObj *cntxt) |
| Reset ground plane estimation parameters. More... | |