81 #ifndef MMALIB_LINALG_MATRIXTRANSPOSE_IXX_OXX_H_
82 #define MMALIB_LINALG_MATRIXTRANSPOSE_IXX_OXX_H_
84 #include "../../common/MMALIB_types.h"
201 void *restrict pOut);
221 const void *restrict pIn,
222 const void *restrict pOut);
MMALIB_STATUS_NAME
The enumeration of all status codes.
void * MMALIB_kernelHandle
Handle type for MMALIB operations.
int32_t MMALIB_LINALG_matrixTranspose_ixX_oxX_getHandleSize(MMALIB_LINALG_matrixTranspose_ixX_oxX_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
MMALIB_STATUS MMALIB_LINALG_matrixTranspose_ixX_oxX_exec_checkParams(MMALIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to MMALIB_LINALG_matrixTranspose_ixX_oxX_e...
MMALIB_STATUS MMALIB_LINALG_matrixTranspose_ixX_oxX_exec(MMALIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel compute function.
MMALIB_STATUS MMALIB_LINALG_matrixTranspose_ixX_oxX_init_checkParams(MMALIB_kernelHandle handle, const MMALIB_bufParams2D_t *bufParamsIn, const MMALIB_bufParams2D_t *bufParamsOut, const MMALIB_LINALG_matrixTranspose_ixX_oxX_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to MMALIB_LINALG_matrixTranspose_ixX_oxX_i...
MMALIB_STATUS MMALIB_LINALG_matrixTranspose_ixX_oxX_init(MMALIB_kernelHandle handle, MMALIB_bufParams2D_t *bufParamsIn, MMALIB_bufParams2D_t *bufParamsOut, MMALIB_LINALG_matrixTranspose_ixX_oxX_InitArgs *pKerInitArgs)
This function should be called before the MMALIB_LINALG_matrixTranspose_ixX_oxX_exec function is call...
Structure containing the parameters to initialize the kernel.
int8_t funcStyle
Variant of the function refer to MMALIB_FUNCTION_STYLE
A structure for a 2 dimensional buffer descriptor.