![]() |
MCUSW
|
Structure containing parameters for ADC MCAL channel configuration. In term of ADC hardware, this represents the step configuration. There are ADC_NUM_CHANNEL steps in the ADC hardware and each step could be mapped to an actual hardware input channel.
Data Fields | |
| uint32 | hwChannelId |
| uint32 | openDelay |
| uint32 | sampleDelay |
| uint32 | rangeCheckEnable |
| Adc_AveragingMode | averagingMode |
| uint32 Adc_ChannelConfigType::hwChannelId |
The hardware channel number from which input is given. Valid values: ADC_MIN_HW_CHANNEL_ID to ADC_MAX_HW_CHANNEL_ID 0x0 = Channel 1 0x1 = Channel 2 0x2 = Channel 3 0x3 = Channel 4 0x4 = Channel 5 0x5 = Channel 6 0x6 = Channel 7 0x7 = Channel 8 0x8 = VREFP 0x9 = VREFN
| uint32 Adc_ChannelConfigType::openDelay |
Number of ADC clock cycles to wait after applying the step configuration registers and before sending the start of ADC conversion. Valid values: ADC_MIN_OPEN_DELAY to ADC_MAX_OPEN_DELAY
| uint32 Adc_ChannelConfigType::sampleDelay |
Number of ADC clock cycles to hold SOC high. The actual delay is +1 of this value. Valid values: ADC_MIN_SAMPLE_DELAY to ADC_MAX_SAMPLE_DELAY
| uint32 Adc_ChannelConfigType::rangeCheckEnable |
Option to enable range check per channel. Enabled if it is TRUE Disabled if it is FALSE
Note: Since there are no standard MCAL API for this feature, this is not supported by the ADC driver. So set this to FALSE
| Adc_AveragingMode Adc_ChannelConfigType::averagingMode |
Option for averaging the sampled data. Refer enum Adc_AveragingMode