![]() |
TI J721E Imaging User Guide
|
Sensor Information structure.
Data Fields | |
| tivx_raw_image_create_params_t | raw_params |
| uint32_t | features |
| uint32_t | aewbMode |
| uint32_t | fps |
| uint32_t | numDataLanes |
| uint32_t | dataLanesMap [4] |
| uint32_t | dataLanesPolarity [4] |
| uint32_t | csi_laneBandSpeed |
| tivx_raw_image_create_params_t IssSensor_Info::raw_params |
raw parameters of the sensor
| uint32_t IssSensor_Info::features |
Bitwise list of feature supported by the sensor
| uint32_t IssSensor_Info::aewbMode |
AEWB mode
| uint32_t IssSensor_Info::fps |
frame rate
| uint32_t IssSensor_Info::numDataLanes |
Number of CSIRX data lanes
| uint32_t IssSensor_Info::dataLanesMap[4] |
Data Lanes map array
| uint32_t IssSensor_Info::dataLanesPolarity[4] |
Data Lanes map array
| uint32_t IssSensor_Info::csi_laneBandSpeed |
CSI2 Rx Lane Band Speed CSI clock