![]() |
TI J721E Imaging User Guide
|
Init Parameters required to allocate SDE driver. This should be identical to Vhwa_m2mSdeSl2AllocPrms. It is defined locally for application to use the same params.
struct App_m2mSdeSl2AllocPrms
Data Fields | |
| uint32_t | maxImgWidth |
| uint32_t | inCcsf |
| uint32_t | searchRange |
| uint32_t | disBuffDepth |
| uint32_t App_M2mSdeSl2AllocPrms::maxImgWidth |
These parameters are used by the driver to allocater SL2 memory, used all driver handles. Ensure to allocate max of all handles requirement.Maximun image width
| uint32_t App_M2mSdeSl2AllocPrms::inCcsf |
CCSF for input image
| uint32_t App_M2mSdeSl2AllocPrms::searchRange |
Search range refer to SDE_DispSearchRange
| uint32_t App_M2mSdeSl2AllocPrms::disBuffDepth |
Maximum disparity buffer depth