![]() |
TI J721E Imaging User Guide
|
Wrapper API's to use TCP/IP sockets
Go to the source code of this file.
Data Structures | |
| struct | Network_SockObj |
Typedefs | |
| typedef int | Bool |
Functions | |
| int32_t | Network_open (Network_SockObj *pObj, uint32_t port) |
| int32_t | Network_close (Network_SockObj *pObj, Bool closeServerSock) |
| int32_t | Network_waitConnect (Network_SockObj *pObj, uint32_t timeout) |
| int32_t | Network_read (Network_SockObj *pObj, uint8_t *dataBuf, uint32_t *dataSize) |
| int32_t | Network_write (Network_SockObj *pObj, uint8_t *dataBuf, uint32_t dataSize) |
| typedef int Bool |
| int32_t Network_open | ( | Network_SockObj * | pObj, |
| uint32_t | port | ||
| ) |
| int32_t Network_close | ( | Network_SockObj * | pObj, |
| Bool | closeServerSock | ||
| ) |
| int32_t Network_waitConnect | ( | Network_SockObj * | pObj, |
| uint32_t | timeout | ||
| ) |
| int32_t Network_read | ( | Network_SockObj * | pObj, |
| uint8_t * | dataBuf, | ||
| uint32_t * | dataSize | ||
| ) |
| int32_t Network_write | ( | Network_SockObj * | pObj, |
| uint8_t * | dataBuf, | ||
| uint32_t | dataSize | ||
| ) |