![]() |
FFTLIB User Guide
|
A structure for a 3 dimensional buffer descriptor.
Definition at line 103 of file FFTLIB_bufParams.h.
Data Fields | |
| uint32_t | data_type |
| Values are of type FFTLIB_data_type_e. More... | |
| uint32_t | dim_x |
| Width of buffer in X dimension in elements. More... | |
| uint32_t | dim_y |
| Height of buffer in Y dimension in elements. More... | |
| int32_t | stride_y |
| Stride in Y dimension in bytes. More... | |
| uint32_t | dim_z |
| Depth of patch in Z dimension in elements. More... | |
| int32_t | stride_z |
| Stride in Z dimension in bytes. More... | |
| uint32_t FFTLIB_bufParams3D_t::data_type |
Values are of type FFTLIB_data_type_e.
Definition at line 105 of file FFTLIB_bufParams.h.
| uint32_t FFTLIB_bufParams3D_t::dim_x |
Width of buffer in X dimension in elements.
Definition at line 107 of file FFTLIB_bufParams.h.
| uint32_t FFTLIB_bufParams3D_t::dim_y |
Height of buffer in Y dimension in elements.
Definition at line 109 of file FFTLIB_bufParams.h.
| int32_t FFTLIB_bufParams3D_t::stride_y |
Stride in Y dimension in bytes.
Definition at line 110 of file FFTLIB_bufParams.h.
| uint32_t FFTLIB_bufParams3D_t::dim_z |
Depth of patch in Z dimension in elements.
Definition at line 112 of file FFTLIB_bufParams.h.
| int32_t FFTLIB_bufParams3D_t::stride_z |
Stride in Z dimension in bytes.
Definition at line 113 of file FFTLIB_bufParams.h.