37 #ifndef COMMON_FFTLIB_UTIL_ZEROBLOAD_H_
38 #define COMMON_FFTLIB_UTIL_ZEROBLOAD_H_ 1
64 __mma_vec zeroVect = (__mma_vec)(0x00);
66 for(r = 0; r < numRows; r++){
78 __mma_vec zeroVect = (__mma_vec)(0);
81 for(r = 0; r < numRows; r++){
90 template <
int32_t UNROLL_TIMES>
94 __mma_vec zeroVect = (__mma_vec)(0);
97 FFTLIB_UNROLL(UNROLL_TIMES)
98 for(r = 0; r < numRows; r++){
static void FFTLIB_UTIL_zeroBload_unroll(int32_t numRows)
static void FFTLIB_UTIL_zeroBload(int32_t numRows)
load numRows of B into the Bload buffer
static void FFTLIB_UTIL_zeroBload_unroll32(int32_t numRows)