![]() |
FFTLIB User Guide
|
Go to the source code of this file.
Functions | |
| static void | FFTLIB_UTIL_SE1Bload (int32_t numRows) |
| load numRows of B into the Bload buffer More... | |
|
inlinestatic |
load numRows of B into the Bload buffer
use streaming engine 1 to load numRows of B into the Bload buffer
| numRows |
Definition at line 61 of file FFTLIB_UTIL_SE1Bload.h.