Go to the source code of this file.
◆ FFTLIB_UTIL_SE0AloadComputeC()
| static void FFTLIB_UTIL_SE0AloadComputeC |
( |
int32_t |
numRows | ) |
|
|
inlinestatic |
use streaming engine 0 to load numRows of A compute C(row) = A(row) x Bfore(:,:)
- Parameters
-
- Returns
- void
Definition at line 65 of file FFTLIB_UTIL_SE0AloadComputeC.h.
◆ FFTLIB_UTIL_SE0AloadComputeC_unroll16()
| static void FFTLIB_UTIL_SE0AloadComputeC_unroll16 |
( |
int32_t |
numRows | ) |
|
|
inlinestatic |
◆ FFTLIB_UTIL_SE0AloadComputeC_unroll32()
| static void FFTLIB_UTIL_SE0AloadComputeC_unroll32 |
( |
int32_t |
numRows | ) |
|
|
inlinestatic |
◆ FFTLIB_UTIL_SE0AloadComputeC_unroll64()
| static void FFTLIB_UTIL_SE0AloadComputeC_unroll64 |
( |
int32_t |
numRows | ) |
|
|
inlinestatic |