![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 193 of file DSPLIB_svd_small_priv.h.
Data Fields | |
| pFxnDSPLIB_svd_small_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_svd_small_exec_cn and DSPLIB_svd_small_exec_ci. More... | |
| uint32_t | widthIn |
| Size of input buffer for different batches DSPLIB_svd_small_init that will be retrieved and used by DSPLIB_svd_small_exec More... | |
| uint32_t | heightIn |
| Height of input data matrix More... | |
| int32_t | strideIn |
| Stride between rows of input data matrix More... | |
| uint32_t | strideU |
| Stride between rows of U matrix More... | |
| uint32_t | strideV |
| Stride between rows of V matrix More... | |
| uint32_t | strideURows |
| uint32_t | strideVRows |
| uint32_t | enableReducedForm |
| Flag for enabling the calculation of reduced form enableReducedForm = 1 for reduced form SVD calc enableReducedForm = 0 for normal SVD calc More... | |
| uint32_t | data_type |
| Data Type. More... | |
| uint8_t | bufPblock [DSPLIB_SVD_SMALL_IXX_IXX_OXX_PBLOCK_SIZE] |
| Buffer to save SE & SA configuration parameters More... | |
| pFxnDSPLIB_svd_small_exec DSPLIB_svd_small_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_svd_small_exec_cn and DSPLIB_svd_small_exec_ci.
Definition at line 197 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::widthIn |
Size of input buffer for different batches DSPLIB_svd_small_init that will be retrieved and used by DSPLIB_svd_small_exec
Width of input data matrix
Definition at line 202 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::heightIn |
Height of input data matrix
Definition at line 204 of file DSPLIB_svd_small_priv.h.
| int32_t DSPLIB_svd_small_PrivArgs::strideIn |
Stride between rows of input data matrix
Definition at line 206 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::strideU |
Stride between rows of U matrix
Definition at line 208 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::strideV |
Stride between rows of V matrix
Definition at line 210 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::strideURows |
Definition at line 211 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::strideVRows |
Definition at line 212 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::enableReducedForm |
Flag for enabling the calculation of reduced form enableReducedForm = 1 for reduced form SVD calc enableReducedForm = 0 for normal SVD calc
Definition at line 216 of file DSPLIB_svd_small_priv.h.
| uint32_t DSPLIB_svd_small_PrivArgs::data_type |
Data Type.
Definition at line 218 of file DSPLIB_svd_small_priv.h.
| uint8_t DSPLIB_svd_small_PrivArgs::bufPblock[DSPLIB_SVD_SMALL_IXX_IXX_OXX_PBLOCK_SIZE] |
Buffer to save SE & SA configuration parameters
Definition at line 220 of file DSPLIB_svd_small_priv.h.