DSPLIB User Guide
DSPLIB_mat_submat_copyInitArgs Struct Reference

Detailed Description

Structure containing the parameters to initialize the kernel.

Definition at line 117 of file DSPLIB_mat_submat_copy.h.

Data Fields

int8_t funcStyle
 Variant of the function refer to DSPLIB_FUNCTION_STYLE
More...
 
uint32_t dimX
 The number of columns in X matrix. More...
 
uint32_t dimY
 The number of rows in X matrix. More...
 
uint32_t dir
 Direction of the data flow
More...
 
uint32_t stRow
 Copying starting from stRow row of matrix
More...
 
uint32_t stCol
 Copying starting from stCol column of matrix
More...
 
uint32_t nRows
 The number of rows to be copied
More...
 
uint32_t nCols
 The number of coulmns to be copied
More...
 

Field Documentation

◆ funcStyle

int8_t DSPLIB_mat_submat_copyInitArgs::funcStyle

Variant of the function refer to DSPLIB_FUNCTION_STYLE

Definition at line 119 of file DSPLIB_mat_submat_copy.h.

◆ dimX

uint32_t DSPLIB_mat_submat_copyInitArgs::dimX

The number of columns in X matrix.

Definition at line 121 of file DSPLIB_mat_submat_copy.h.

◆ dimY

uint32_t DSPLIB_mat_submat_copyInitArgs::dimY

The number of rows in X matrix.

Definition at line 123 of file DSPLIB_mat_submat_copy.h.

◆ dir

uint32_t DSPLIB_mat_submat_copyInitArgs::dir

Direction of the data flow

Definition at line 125 of file DSPLIB_mat_submat_copy.h.

◆ stRow

uint32_t DSPLIB_mat_submat_copyInitArgs::stRow

Copying starting from stRow row of matrix

Definition at line 127 of file DSPLIB_mat_submat_copy.h.

◆ stCol

uint32_t DSPLIB_mat_submat_copyInitArgs::stCol

Copying starting from stCol column of matrix

Definition at line 129 of file DSPLIB_mat_submat_copy.h.

◆ nRows

uint32_t DSPLIB_mat_submat_copyInitArgs::nRows

The number of rows to be copied

Definition at line 131 of file DSPLIB_mat_submat_copy.h.

◆ nCols

uint32_t DSPLIB_mat_submat_copyInitArgs::nCols

The number of coulmns to be copied

Definition at line 133 of file DSPLIB_mat_submat_copy.h.