![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 170 of file DSPLIB_fir_priv.h.
Data Fields | |
| DSPLIB_fir_InitArgs | initArgs |
| Structure holding initialization parameters More... | |
| pFxnDSPLIB_fir_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_fir_exec_cn and DSPLIB_fir_exec_ci. More... | |
| uint32_t | dataBufferInPitch |
| Pitch of input buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB_fir_exec More... | |
| uint32_t | dataBufferOutPitch |
| Pitch of output buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB_fir_exec More... | |
| uint32_t | filterPitch |
| Pitch of filter coefficient buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB_fir_exec More... | |
| uint32_t | flag |
| Array to store the configuration prepared by DSPLIB_fir_init_ci that will be retrieved and used by DSPLIB_fir_exec_ci More... | |
| int32_t | dataLoopSize |
| int32_t | outputSize |
| int32_t | filterLoopSize |
| int32_t | remFilterLoopSize |
| uint8_t | bufPblock [DSPLIB_FIR_IXX_IXX_OXX_PBLOCK_SIZE] |
| DSPLIB_fir_InitArgs DSPLIB_fir_PrivArgs::initArgs |
Structure holding initialization parameters
Definition at line 172 of file DSPLIB_fir_priv.h.
| pFxnDSPLIB_fir_exec DSPLIB_fir_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_fir_exec_cn and DSPLIB_fir_exec_ci.
Definition at line 176 of file DSPLIB_fir_priv.h.
| uint32_t DSPLIB_fir_PrivArgs::dataBufferInPitch |
Pitch of input buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB_fir_exec
Definition at line 180 of file DSPLIB_fir_priv.h.
| uint32_t DSPLIB_fir_PrivArgs::dataBufferOutPitch |
Pitch of output buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB_fir_exec
Definition at line 184 of file DSPLIB_fir_priv.h.
| uint32_t DSPLIB_fir_PrivArgs::filterPitch |
Pitch of filter coefficient buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB_fir_exec
Definition at line 189 of file DSPLIB_fir_priv.h.
| uint32_t DSPLIB_fir_PrivArgs::flag |
Array to store the configuration prepared by DSPLIB_fir_init_ci that will be retrieved and used by DSPLIB_fir_exec_ci
flag to indicate small or large FIR flag = 0 is small and flag = 1 is large
Definition at line 195 of file DSPLIB_fir_priv.h.
| int32_t DSPLIB_fir_PrivArgs::dataLoopSize |
Definition at line 196 of file DSPLIB_fir_priv.h.
| int32_t DSPLIB_fir_PrivArgs::outputSize |
Definition at line 197 of file DSPLIB_fir_priv.h.
| int32_t DSPLIB_fir_PrivArgs::filterLoopSize |
Definition at line 198 of file DSPLIB_fir_priv.h.
| int32_t DSPLIB_fir_PrivArgs::remFilterLoopSize |
Definition at line 199 of file DSPLIB_fir_priv.h.
| uint8_t DSPLIB_fir_PrivArgs::bufPblock[DSPLIB_FIR_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 200 of file DSPLIB_fir_priv.h.