![]() |
DSPLIB User Guide
|
Kernel for adding two input vector data.
Data Structures | |
| struct | DSPLIB_add_InitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_add_getHandleSize (DSPLIB_add_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_add_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_add_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_add_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_add_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_add_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_add_init function. This function is called with the same parameters as the DSPLIB_add_init, and this function must be called before the DSPLIB_add_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_add_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn1, const void *restrict pIn2, const void *restrict pOut) |
| This function checks the validity of the parameters passed to DSPLIB_add_exec function. This function is called with the same parameters as the DSPLIB_add_init, and this function must be called before the DSPLIB_add_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_add_exec (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut) |
| This function is the main kernel compute function. More... | |
| int32_t DSPLIB_add_getHandleSize | ( | DSPLIB_add_InitArgs * | pKerInitArgs | ) |
This is a query function to calculate the size of internal handle.
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
Definition at line 25 of file DSPLIB_add.cpp.
| DSPLIB_STATUS DSPLIB_add_init | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_add_InitArgs * | pKerInitArgs | ||
| ) |
This function should be called before the DSPLIB_add_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 84 of file DSPLIB_add.cpp.
| DSPLIB_STATUS DSPLIB_add_init_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_add_InitArgs * | pKerInitArgs | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_add_init function. This function is called with the same parameters as the DSPLIB_add_init, and this function must be called before the DSPLIB_add_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 32 of file DSPLIB_add.cpp.
| DSPLIB_STATUS DSPLIB_add_exec_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const void *restrict | pIn1, | ||
| const void *restrict | pIn2, | ||
| const void *restrict | pOut | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_add_exec function. This function is called with the same parameters as the DSPLIB_add_init, and this function must be called before the DSPLIB_add_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn1 | : Pointer to the structure input buffer 1 |
| [in] | pIn2 | : Pointer to the structure input buffer 2 |
| [out] | pout | : Pointer to the output buffer |
Definition at line 64 of file DSPLIB_add.cpp.
| DSPLIB_STATUS DSPLIB_add_exec | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn1, | ||
| void *restrict | pIn2, | ||
| void *restrict | pOut | ||
| ) |
This function is the main kernel compute function.
Please refer to details under DSPLIB_add_exec
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 181 of file DSPLIB_add.cpp.