DSPLIB User Guide
DSPLIB_sqrAdd.cpp
Go to the documentation of this file.
1 /******************************************************************************
2  * *
3  * module name :DSPLIB *
4  * *
5  * module descripton :Matrix Multiply Accelerator Library module for C7x+MMA *
6  * *
7  * Copyright (C) 2017-2018 Texas Instruments Incorporated - https://www.ti.com/ *
8  * ALL RIGHTS RESERVED *
9  * *
10  ******************************************************************************/
11 
23 #include "DSPLIB_sqrAdd_priv.h"
24 
26 {
27  int32_t privBufSize = sizeof(DSPLIB_sqrAdd_PrivArgs);
28  return privBufSize;
29 }
30 
33  const DSPLIB_bufParams1D_t *bufParamsIn,
34  const DSPLIB_bufParams1D_t *bufParamsOut,
35  const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
36 {
38 
39 #if DSPLIB_DEBUGPRINT
40  printf("Enter DSPLIB_sqrAdd_init_checkParams\n");
41 #endif
42  if (handle == NULL) {
43  status = DSPLIB_ERR_NULL_POINTER;
44  }
45 
46  if (status == DSPLIB_SUCCESS) {
47  if ((bufParamsIn->data_type == DSPLIB_UINT8) && (bufParamsOut->data_type == DSPLIB_UINT32)){
48  status = DSPLIB_SUCCESS;
49  }
50  else if ((bufParamsIn->data_type == DSPLIB_INT8) && (bufParamsOut->data_type == DSPLIB_INT32)){
51  status = DSPLIB_SUCCESS;
52  }
53  else if ((bufParamsIn->data_type == DSPLIB_UINT16) && (bufParamsOut->data_type == DSPLIB_UINT64)){
54  status = DSPLIB_SUCCESS;
55  }
56  else if ((bufParamsIn->data_type == DSPLIB_INT16) && (bufParamsOut->data_type == DSPLIB_INT64)){
57  status = DSPLIB_SUCCESS;
58  }
59  else if ((bufParamsIn->data_type == DSPLIB_UINT32) && (bufParamsOut->data_type == DSPLIB_UINT64)){
60  status = DSPLIB_SUCCESS;
61  }
62  else if ((bufParamsIn->data_type == DSPLIB_INT32) && (bufParamsOut->data_type == DSPLIB_INT64)){
63  status = DSPLIB_SUCCESS;
64  }
65  else if ((bufParamsIn->data_type == DSPLIB_FLOAT32) && (bufParamsOut->data_type == DSPLIB_FLOAT32)){
66  status = DSPLIB_SUCCESS;
67  }
68  else if ((bufParamsIn->data_type == DSPLIB_FLOAT64) && (bufParamsOut->data_type == DSPLIB_FLOAT64)){
69  status = DSPLIB_SUCCESS;
70  }
71  else {
72  status = DSPLIB_ERR_INVALID_TYPE;
73  }
74  }
75 
76  return status;
77 }
78 
80 DSPLIB_sqrAdd_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
81 {
82  DSPLIB_STATUS status;
83 
84 #if DSPLIB_DEBUGPRINT
85  printf("Enter DSPLIB_sqrAdd_exec_checkParams\n");
86 #endif
87  if ((pIn == NULL) || (pOut == NULL)) {
88  status = DSPLIB_ERR_NULL_POINTER;
89  }
90  else {
91  status = DSPLIB_SUCCESS;
92  }
93 
94  return status;
95 }
96 
98  DSPLIB_bufParams1D_t *bufParamsIn,
99  DSPLIB_bufParams1D_t *bufParamsOut,
100  const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
101 {
102  DSPLIB_STATUS status = DSPLIB_SUCCESS;
103  DSPLIB_sqrAdd_PrivArgs *pKerPrivArgs = (DSPLIB_sqrAdd_PrivArgs *) handle;
104 
105 #if DSPLIB_DEBUGPRINT
106  printf("DSPLIB_DEBUGPRINT Enter DSPLIB_sqrAdd_init\n");
107 #endif
108  pKerPrivArgs->blockSize = pKerInitArgs->dataSize;
109 
110 #if DSPLIB_DEBUGPRINT
111  printf("DSPLIB_DEBUGPRINT DSPLIB_sqrAdd_init pKerPrivArgs->blockSize %d "
112  "bufParamsIn->data_type %d\n",
113  pKerPrivArgs->blockSize, bufParamsIn->data_type);
114 #endif
115 
116  if (pKerInitArgs->funcStyle == DSPLIB_FUNCTION_NATC) {
117  if (bufParamsIn->data_type == DSPLIB_FLOAT32) {
118  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_cn<float>;
119  }
120  else if (bufParamsIn->data_type == DSPLIB_FLOAT64) {
121  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_cn<double>;
122  }
123  else if (bufParamsIn->data_type == DSPLIB_INT8) {
124  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_cn<int8_t>;
125  }
126  else if (bufParamsIn->data_type == DSPLIB_UINT8) {
127  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_cn<uint8_t>;
128  }
129  else if (bufParamsIn->data_type == DSPLIB_INT16) {
130  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_cn<int16_t>;
131  }
132  else if (bufParamsIn->data_type == DSPLIB_UINT16) {
134  }
135  else if (bufParamsIn->data_type == DSPLIB_INT32) {
136  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_cn<int32_t>;
137  }
138  else if (bufParamsIn->data_type == DSPLIB_UINT32) {
140  }
141  else {
142  status = DSPLIB_ERR_INVALID_TYPE;
143 #if DSPLIB_DEBUGPRINT
144  printf("DSPLIB_DEBUGPRINT CP 2 status %d\n", status);
145 #endif
146  }
147  }
148  else {
149  if (bufParamsIn->data_type == DSPLIB_FLOAT32) {
150 #if DSPLIB_DEBUGPRINT
151  printf("DSPLIB_DEBUGPRINT bufParamsIn->data_type == DSPLIB_FLOAT32\n");
152 #endif
153  status = DSPLIB_sqrAdd_init_ci<float>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
154  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_ci<float>;
155  }
156  else if (bufParamsIn->data_type == DSPLIB_FLOAT64) {
157  status = DSPLIB_sqrAdd_init_ci<double>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
158  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_ci<double>;
159  }
160  else if (bufParamsIn->data_type == DSPLIB_INT8) {
161  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_ci<int8_t>;
162  status = DSPLIB_sqrAdd_init_ci<int8_t>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
163  }
164  else if (bufParamsIn->data_type == DSPLIB_UINT8) {
165  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_ci<uint8_t>;
166  status = DSPLIB_sqrAdd_init_ci<uint8_t>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
167  }
168  else if (bufParamsIn->data_type == DSPLIB_INT16) {
169  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_ci<int16_t>;
170  status = DSPLIB_sqrAdd_init_ci<int16_t>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
171  }
172  else if (bufParamsIn->data_type == DSPLIB_UINT16) {
174  status = DSPLIB_sqrAdd_init_ci<uint16_t>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
175  }
176  else if (bufParamsIn->data_type == DSPLIB_INT32) {
177  pKerPrivArgs->execute = DSPLIB_sqrAdd_exec_ci<int32_t>;
178  status = DSPLIB_sqrAdd_init_ci<int32_t>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
179  }
180  else if (bufParamsIn->data_type == DSPLIB_UINT32) {
182  status = DSPLIB_sqrAdd_init_ci<uint32_t>(handle, bufParamsIn, bufParamsOut, pKerInitArgs);
183  }
184  else {
185  status = DSPLIB_ERR_INVALID_TYPE;
186 #if DSPLIB_DEBUGPRINT
187  printf("DSPLIB_DEBUGPRINT CP 2 status %d\n", status);
188 #endif
189  }
190  }
191 #if DSPLIB_DEBUGPRINT
192  printf("DSPLIB_DEBUGPRINT CP 3 status %d\n", status);
193 #endif
194  return status;
195 }
196 
197 DSPLIB_STATUS DSPLIB_sqrAdd_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
198 {
199  DSPLIB_STATUS status;
200 
201 #if DSPLIB_DEBUGPRINT
202  printf("DSPLIB_DEBUGPRINT Enter DSPLIB_sqrAdd_exec\n");
203 #endif
204 
205  DSPLIB_sqrAdd_PrivArgs *pKerPrivArgs = (DSPLIB_sqrAdd_PrivArgs *) handle;
206 
207 #if DSPLIB_DEBUGPRINT
208  printf("DSPLIB_DEBUGPRINT pKerPrivArgs->blockSize %d\n", pKerPrivArgs->blockSize);
209 #endif
210  status = pKerPrivArgs->execute(handle, pIn, pOut);
211 
212  return status;
213 }
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< double >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< float >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< double >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< int8_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< int16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< int16_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< uint8_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< uint32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< int32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< uint16_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< int32_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< uint16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_ci< uint32_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< int8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_sqrAdd_init_ci< uint8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint16_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int32_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int8_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint8_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< double >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< float >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< int16_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_sqrAdd_exec_cn< uint32_t >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_sqrAdd.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
Definition: DSPLIB_types.h:151
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
Definition: DSPLIB_types.h:172
@ DSPLIB_FUNCTION_NATC
Definition: DSPLIB_types.h:176
@ DSPLIB_UINT64
@ DSPLIB_UINT8
@ DSPLIB_UINT16
@ DSPLIB_INT32
@ DSPLIB_INT16
@ DSPLIB_FLOAT32
@ DSPLIB_INT64
@ DSPLIB_FLOAT64
@ DSPLIB_UINT32
@ DSPLIB_INT8
@ DSPLIB_SUCCESS
Definition: DSPLIB_types.h:152
@ DSPLIB_ERR_NULL_POINTER
Definition: DSPLIB_types.h:157
@ DSPLIB_ERR_INVALID_TYPE
Definition: DSPLIB_types.h:155
int32_t DSPLIB_sqrAdd_getHandleSize(DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_sqrAdd_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_sqrAdd_exec function....
DSPLIB_STATUS DSPLIB_sqrAdd_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_sqrAdd_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_sqrAdd_init function....
DSPLIB_STATUS DSPLIB_sqrAdd_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_sqrAdd_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_sqrAdd_exec function is called. This function takes ...
A structure for a 1 dimensional buffer descriptor.
uint32_t data_type
Values are of type DSPLIB_data_type_e.
Structure containing the parameters to initialize the kernel.
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
uint32_t dataSize
Size of input data
Structure that is reserved for internal use by the kernel.
pFxnDSPLIB_sqrAdd_exec execute
Function pointer to point to the right execution variant between DSPLIB_sqrAdd_exec_cn and DSPLIB_sqr...
int32_t blockSize
Size of input buffer for different batches DSPLIB_sqrAdd_init that will be retrieved and used by DSPL...