DSPLIB User Guide
DSPLIB_qrd_priv.h File Reference

Introduction

Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_qrd.

Definition in file DSPLIB_qrd_priv.h.

Go to the source code of this file.

Data Structures

struct  DSPLIB_qrd_PrivArgs
 Structure that is reserved for internal use by the kernel. More...
 

Macros

#define DSPLIB_QRD_IXX_IXX_OXX_PBLOCK_SIZE   (20 * SE_PARAM_SIZE)
 Macro to define the size of bufPblock array of DSPLIB_qrd_PrivArgs structure. More...
 

Typedefs

typedef DSPLIB_STATUS(* pFxnDSPLIB_qrd_exec) (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch)
 This is a function pointer type that conforms to the declaration of DSPLIB_qrd_exec_ci and DSPLIB_qrd_exec_cn. More...
 

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_init_ci (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsU, const DSPLIB_qrdInitArgs *pKerInitArgs)
 This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_exec_ci (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch)
 This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_exec. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsA, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams1D_t *bufParamsU, const DSPLIB_qrdInitArgs *pKerInitArgs)
 This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_exec_cn (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_exec. More...
 
template<typename dataType >
void DSPLIB_qrd_blk_move_init_ci (DSPLIB_kernelHandle handle)
 
template<typename dataType >
void DSPLIB_qrd_alpha_init_ci (DSPLIB_kernelHandle handle)
 
template<typename dataType >
void DSPLIB_R_column_init_ci (DSPLIB_kernelHandle handle)
 
template<typename dataType >
void DSPLIB_Q_matrix_init_ci (DSPLIB_kernelHandle handle)
 
template<typename dataType >
void DSPLIB_qrd_R_matrix_exec_ci (dataType *pLocalR, dataType *pLocalU, dataType *pSum, dataType scale, int32_t colStrideR, int32_t nRows, int32_t nCols, uint8_t *pBlock)
 
template<typename dataType >
void DSPLIB_qrd_Q_matrix_exec_ci (dataType *pLocalQ, dataType *pLocalU, dataType *pSum, dataType scale, int32_t colStrideQ, int32_t nRows, int32_t nCols, uint8_t *pBlock)
 

Macro Definition Documentation

◆ DSPLIB_QRD_IXX_IXX_OXX_PBLOCK_SIZE

#define DSPLIB_QRD_IXX_IXX_OXX_PBLOCK_SIZE   (20 * SE_PARAM_SIZE)

Macro to define the size of bufPblock array of DSPLIB_qrd_PrivArgs structure.

Definition at line 40 of file DSPLIB_qrd_priv.h.

Typedef Documentation

◆ pFxnDSPLIB_qrd_exec

typedef DSPLIB_STATUS(* pFxnDSPLIB_qrd_exec) (DSPLIB_kernelHandle handle, const void *restrict pA, const void *restrict pQ, const void *restrict pR, const void *restrict pU, const void *restrict pScratch)

This is a function pointer type that conforms to the declaration of DSPLIB_qrd_exec_ci and DSPLIB_qrd_exec_cn.

Definition at line 47 of file DSPLIB_qrd_priv.h.

Function Documentation

◆ DSPLIB_qrd_init_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_init_ci ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams2D_t bufParamsA,
DSPLIB_bufParams2D_t bufParamsQ,
DSPLIB_bufParams2D_t bufParamsR,
DSPLIB_bufParams1D_t bufParamsU,
const DSPLIB_qrdInitArgs pKerInitArgs 
)

This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_init.

This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_qrd_exec_ci would be called later independently by the application. When DSPLIB_qrd_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_qrd_exec_ci does not lose cycles to determine the hardware configuration.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsA: Pointer to the structure containing dimensional information of input matrix
[out]bufParamsQ: Pointer to the structure containing dimensional information of Q matrix
[out]bufParamsR: Pointer to the structure containing dimensional information of R matrix
[in]bufParamsU: Pointer to the structure containing dimensional information of temporary vector U.
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 86 of file DSPLIB_qrd_ci.cpp.

◆ DSPLIB_qrd_exec_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_exec_ci ( DSPLIB_kernelHandle  handle,
const void *restrict  pA,
const void *restrict  pQ,
const void *restrict  pR,
const void *restrict  pU,
const void *restrict  pScratch 
)

This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_exec.

The function permforms the optimized QR decomposition.

Parameters
[in]handle: Active handle to the kernel
[in]pA: Pointer to the input matrix
[out]pQ: Pointer to the output matrix Q
[out]pR: Pointer to the output matrix R
[in]pU: Pointer to the temporary vector
[in]pScratchPointer to the Scratch buffer
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned

Definition at line 370 of file DSPLIB_qrd_ci.cpp.

◆ DSPLIB_qrd_init_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_init_cn ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams2D_t bufParamsA,
DSPLIB_bufParams2D_t bufParamsQ,
DSPLIB_bufParams2D_t bufParamsR,
DSPLIB_bufParams1D_t bufParamsU,
const DSPLIB_qrdInitArgs pKerInitArgs 
)

This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_init.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsA: Pointer to the structure containing dimensional information of input matrix
[out]bufParamsQ: Pointer to the structure containing dimensional information of Q matrix
[out]bufParamsR: Pointer to the structure containing dimensional information of R matrix
[in]bufParamsU: Pointer to the structure containing dimensional information of temporary vector U.
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 44 of file DSPLIB_qrd_cn.cpp.

◆ DSPLIB_qrd_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_qrd_exec_cn ( DSPLIB_kernelHandle  handle,
const void *restrict  pA,
const void *restrict  pQ,
const void *restrict  pR,
const void *restrict  pU,
const void *restrict  pScratch 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_qrd_exec.

Parameters
[in]handle: Active handle to the kernel
[in]pA: Pointer to the input matrix
[out]pQ: Pointer to the output matrix Q
[out]pR: Pointer to the output matrix R
[in]pU: Pointer to the temporary vector
[in]pScratchPointer to the Scratch buffer
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 75 of file DSPLIB_qrd_cn.cpp.

◆ DSPLIB_qrd_blk_move_init_ci()

template<typename dataType >
void DSPLIB_qrd_blk_move_init_ci ( DSPLIB_kernelHandle  handle)

◆ DSPLIB_qrd_alpha_init_ci()

template<typename dataType >
void DSPLIB_qrd_alpha_init_ci ( DSPLIB_kernelHandle  handle)

Definition at line 43 of file DSPLIB_qrd_ci.cpp.

◆ DSPLIB_R_column_init_ci()

template<typename dataType >
void DSPLIB_R_column_init_ci ( DSPLIB_kernelHandle  handle)

Definition at line 41 of file DSPLIB_qrd_ci_opt.cpp.

◆ DSPLIB_Q_matrix_init_ci()

template<typename dataType >
void DSPLIB_Q_matrix_init_ci ( DSPLIB_kernelHandle  handle)

Definition at line 62 of file DSPLIB_qrd_ci_opt.cpp.

◆ DSPLIB_qrd_R_matrix_exec_ci()

template<typename dataType >
void DSPLIB_qrd_R_matrix_exec_ci ( dataType *  pLocalR,
dataType *  pLocalU,
dataType *  pSum,
dataType  scale,
int32_t  colStrideR,
int32_t  nRows,
int32_t  nCols,
uint8_t *  pBlock 
)

Definition at line 242 of file DSPLIB_qrd_ci_opt.cpp.

◆ DSPLIB_qrd_Q_matrix_exec_ci()

template<typename dataType >
void DSPLIB_qrd_Q_matrix_exec_ci ( dataType *  pLocalQ,
dataType *  pLocalU,
dataType *  pSum,
dataType  scale,
int32_t  colStrideQ,
int32_t  nRows,
int32_t  nCols,
uint8_t *  pBlock 
)

Definition at line 1024 of file DSPLIB_qrd_ci_opt.cpp.