40 printf(
"Enter DSPLIB_negate_init_checkParams\n");
71 printf(
"Enter DSPLIB_negate_exec_checkParams\n");
73 if ((pIn == NULL) || (pOut == NULL)) {
92 printf(
"DSPLIB_DEBUGPRINT Enter DSPLIB_negate_init\n");
97 printf(
"DSPLIB_DEBUGPRINT DSPLIB_negate_init pKerPrivArgs->blockSize %d "
98 "bufParamsIn->data_type %d\n",
114 #if DSPLIB_DEBUGPRINT
115 printf(
"DSPLIB_DEBUGPRINT CP 2 status %d\n", status);
136 #if DSPLIB_DEBUGPRINT
137 printf(
"DSPLIB_DEBUGPRINT CP 2 status %d\n", status);
141 #if DSPLIB_DEBUGPRINT
142 printf(
"DSPLIB_DEBUGPRINT CP 3 status %d\n", status);
151 #if DSPLIB_DEBUGPRINT
152 printf(
"DSPLIB_DEBUGPRINT Enter DSPLIB_negate_exec\n");
157 #if DSPLIB_DEBUGPRINT
158 printf(
"DSPLIB_DEBUGPRINT pKerPrivArgs->blockSize %d\n", pKerPrivArgs->
blockSize);
160 status = pKerPrivArgs->
execute(handle, pIn, pOut);
template DSPLIB_STATUS DSPLIB_negate_exec_ci< int16_t, DSPLIB_INT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_negate_exec_ci< int32_t, DSPLIB_INT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_negate_exec_ci< int8_t, DSPLIB_INT8 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_negate_init_ci< int32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_negate_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_negate_init_ci< int8_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_negate_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_negate_init_ci< int16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_negate_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_negate_exec_cn< int8_t, DSPLIB_INT8 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_negate_exec_cn< int16_t, DSPLIB_INT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_negate_exec_cn< int32_t, DSPLIB_INT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_negate.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
@ DSPLIB_ERR_NULL_POINTER
@ DSPLIB_ERR_INVALID_TYPE
DSPLIB_STATUS DSPLIB_negate_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_negate_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_negate_exec function is called. This function takes ...
int32_t DSPLIB_negate_getHandleSize(DSPLIB_negate_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_negate_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_negate_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_negate_init function....
DSPLIB_STATUS DSPLIB_negate_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_negate_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_negate_exec function....
A structure for a 1 dimensional buffer descriptor.
uint32_t data_type
Values are of type DSPLIB_data_type_e.
Structure containing the parameters to initialize the kernel.
uint32_t dataSize
Size of input data
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
Structure that is reserved for internal use by the kernel.
int32_t blockSize
Size of input buffer for different batches DSPLIB_negate_init that will be retrieved and used by DSPL...
pFxnDSPLIB_negate_exec execute
Function pointer to point to the right execution variant between DSPLIB_negate_exec_cn and DSPLIB_neg...