81 #ifndef DSPLIB_MUL_IXX_IXX_OXX_H_
82 #define DSPLIB_MUL_IXX_IXX_OXX_H_
84 #include "../common/DSPLIB_types.h"
190 const void *restrict pIn1,
191 const void *restrict pIn2,
192 const void *restrict pOut);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_mul_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_mul_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_mul_init function....
DSPLIB_STATUS DSPLIB_mul_exec(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_mul_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_mul_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_mul_exec function is called. This function takes car...
int32_t DSPLIB_mul_getHandleSize(DSPLIB_mul_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_mul_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn1, const void *restrict pIn2, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_mul_exec function....
A structure for a 1 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
uint32_t dataSize
Size of input data
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE