DSPLIB User Guide
DSPLIB_minerror.h File Reference

Go to the source code of this file.

Data Structures

struct  DSPLIB_minerror_InitArgs
 Structure containing the parameters to initialize the kernel. More...
 

Functions

int32_t DSPLIB_minerror_getHandleSize (DSPLIB_minerror_InitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_minerror_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsErrCoefs, DSPLIB_bufParams1D_t *bufParamsOutIndex, DSPLIB_bufParams1D_t *bufParamsOutVal, DSPLIB_minerror_InitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_minerror_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_minerror_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsErrCoefs, const DSPLIB_bufParams1D_t *bufParamsOutIndex, const DSPLIB_bufParams1D_t *bufParamsOutVal, const DSPLIB_minerror_InitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_minerror_init function. This function is called with the same parameters as the DSPLIB_minerror_init, and this function must be called before the DSPLIB_minerror_init is called. More...
 
DSPLIB_STATUS DSPLIB_minerror_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pErrCoefs, const int *restrict pMaxIndex, const void *restrict pMaxVal)
 This function checks the validity of the parameters passed to DSPLIB_minerror_exec function. This function is called with the same parameters as the DSPLIB_minerror_init, and this function must be called before the DSPLIB_minerror_init is called. More...
 
DSPLIB_STATUS DSPLIB_minerror_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pErrCoefs, int *restrict pMaxIndex, void *restrict pMaxVal)
 This function is the main kernel compute function. More...